Global site

ABB's website uses cookies. By staying here you are agreeing to our use of cookies. Learn more

ABB i-bus Tool

A professional service tool for KNX system integrators

ABB presents a fully new and innovative software concept with the i-bus Tool. It supports system integrators during commissioning and service of KNX installations. The i-bus Tool accesses one ABB i-bus KNX device via a standard KNX interface (RS232, USB, IP) with the assistance of the physical address. The integrator can trigger the desired functions, read values, simulate states and make settings for the connected device. Internal information and states of the device hardware and software applications, which were not available to the integrators or only available after considerable effort, are now available in a transparent manner and can be specifically retrieved and partly influenced. The information from status bytes can, for example, be represented as plain text.

An important principle is that no divergences to the ETS project can result through the i-bus Tool. The i-bus Tool is optional, so that the ABB i-bus KNX devices are still be commissioned using the ETS.

Diagnostics and Commissioning Support for the Professional

ABB provides a unique user interface within the i-bus Tool, a so-called plug-in, for every supported device. The device-specific information is displayed via this plug-in, and the required settings can be made.
The ABB i-bus Tool is being expanded continuously with new functions and supported devices. The expansions are automatically made available by an online update and can be installed if required.

The i-bus Tool supports the following languages:
Dutch, English, French, German, Italian, Polish, Russian, Spanish
The presentantion language can be changed via "Settings" menu.

The ABB i-bus Tool is free-of-charge.

Latest Plug-In's

Information and Download