Global site

ABB's website uses cookies. By staying here you are agreeing to our use of cookies. Learn more

ArcLimiter for rapid arc fault extinguishing

Maintaining power quality for the upstream processes while extinguishing an arc fault.

With the UFES grounding system operating in <4 milliseconds, the magnitude of the low voltage (LV) fault level becomes a secondary consideration.  

Operating speed becomes the critical parameter as final clearing of fault current falls to the upstream/downstream Current Limiting Fuse (CLF).

When the Primary Switching Elements (PSE) activates, a bolted line-to-ground fault is introduced, dramatically reducing the effects of the LV arc fault condition.  This line-to-ground fault has the potential to be detected by upstream protection relays and begins tripping breakers mere seconds later.  The introduction of CLF in the appropriate location becomes a voltage dip duration device under these conditions. This solution can be accomplished at the low or medium voltage level
and it is type tested according to IEEE C37.20.7
 

Why ABB?

- Greatly increased system and process availability by avoidance of heavy damages inside the switchgear, of the equipment and the direct environment
- Drastic reduction of downtimes and repair costs
- Greatly increased operator safety for switchgears
- Minimization of pressure rise and gases in the faulty compartment and surrounding switchgear building
- Reduction of Voltage Dip duration as seen by upstream devices during fault clearing

Are you looking for support or purchase information?

Loading documents

Get to know more

Related offering