ABB Ability™ mobile gas leak detection

Finds leaks fast and shares data via the Cloud. Improves pipeline integrity and public safety.

-Measure, map, share while driving

-Detect leaks hundreds of meters away

-Compatible with cars, ATV, aircraft, drones

ABB Ability mobile gas leak detection system uses ABB’s patented Off-Axis Integrated Cavity Output Spectroscopy (OA-ICOS) technique which has a sensitivity and precision more than 3000 times greater than legacy methods. This enables identification of leaks several hundred feet away from the source.

Current traditional leak detection technology is slow, laborious and costly. Operators walk on foot near the pipeline with hand-held sensors making paper-based reports.This is slow and can lead to dangerous leaks being missed or not identified in a timely manner. ABB’s Ability mobile gas leak detection system delivers a low cost per leak solution with low false positives. Reporting includes mapping of the leaks available via a mobile app and measurements as Cloud-based service.

The system consists of ABB’s Methane/Ethane Analyzer, a GPS, a sonic anemometer and proprietary leak detection software that presents real-time geospatial maps of multiple gas concentrations in real time. The software’s sophisticated leak detection algorithm combines the system’s measurements of gas concentrations (CH4, C2H6), local coordinates (GPS) and local wind velocity (sonic anemometer) to estimate the location of the leak. Readings are stored in the device and can be transmitted in real-time to the cloud for centralized monitoring.

Typical applications include pipeline monitoring, surveying mains and services, odor investigation, construction verification, post disaster evaluation and frost line evaluation.

About ABB

ABB (ABBN: SIX Swiss Ex) is a pioneering technology leader in electrification products, robotics and motion, industrial automation and power grids serving customers in utilities, industry and transport & infrastructure globally. For more than four decades, ABB is writing the future of industrial digitalization. With more than 70 million devices connected through its installed base of more than 70,000 control systems across all customer segments, ABB is ideally positioned to benefit from the Energy and Fourth Industrial Revolution. With a heritage of more than 130 years, ABB operates in more than 100 countries with about 132,000 employees.www.abb.com

For more information please contact:

ABB Media Relations

Melissa London

Tel: +1 919 649-6581

Melissa.london@us.abb.com

1/1

Share this article

Facebook LinkedIn Twitter