New concept in centralized protection and control for distribution substations

Hanover - SSC600 centralizes all protection and control functionality in a single, IEC 61850-compliant device on substation level to reduce network complexity and support optimal, lifelong asset management for the digital substation.

ABB is introducing an innovative, centralized approach to protection and control in distribution networks, embodied in ABB AbilityTM smart substation control and protection for electrical systems, SSC600. Although representing a new way of thinking, SSC600 builds on ABB’s solid and proven technological foundation manifested in the renowned Relion® protection and control family.

SSC600 has been designed to support the ABB Ability offerings of digitally enabled solutions, helping utilities and industries know more, do more and do it better than before. Combining SSC600 with other ABB Ability products and solutions offers a new way of looking at substation life cycle management. The SSC600 advanced connectivity capabilities enable seamless integration with additional services, such as remote diagnostics, asset management and upgrade services, all for great benefit of the customer.

SSC600 offers extensive application coverage with a single device for convenient station-wide visibility, minimal engineering, easy and cost-efficient process management, and advanced life cycle management for the digital substation. Combining SSC600 with merging units, which provide the measurements and physical interface between the primary equipment in the switchgear and SSC600, creates a unique, IEC 61850-compliant, centralized protection and control solution.

“SSC600 offers a fast, easy and cost-effective way to provide an existing substation with the latest technological developments within protection and control, while leaving the existing relays as backup protection” said Alessandro Palin, Managing Director of ABB’s Distributions Solutions business. “New installations will conveniently only need bay-level merging units in addition to SSC600. Adding a second SSC600 device will create a centralized protection and control solution with full redundancy”.

The modular software allows customization at the initial ordering stage and flexible modification for the lifetime of the digital substation. SSC600 is ready to evolve alongside the grid to adapt to changing protection requirements. Continuous access to new software developments guarantees an always up-to-date substation system. The advantage of only having to modify one device instead of all bay-level protection and control devices makes upgrading the entire substation system easier than ever.

Caruna, the largest distribution system operator in Finland, was looking for a flexible and future-proof solution for their network and chose to pilot ABB’s new smart substation control and protection device. To meet new protection requirements and to benefit from the latest developments in relay technology, SSC600 was installed in Caruna’s substation in Noormarkku.

“SSC600 represents a modern and cost-effective way to detect, locate and isolate faults for the benefit of our customers,” said Sauli Antila, Head of Network Development at Caruna. “SSC600 also provides a convenient platform for creating new functionality to meet future requirements.”

The ability to monitor and control the great variety of substation devices with one single device via a centralized human-machine interface (HMI), translates into increased situational awareness and easy access to valuable power distribution process information.

SSC600 will be showcased at Hannover Messe 2018 at the ABB booth in Hall 11, Stand A35. SSC600 will be released for sale during 2018.

ABB (ABBN: SIX Swiss Ex) is a pioneering technology leader in electrification products, robotics and motion, industrial automation and power grids, serving customers in utilities, industry and transport & infrastructure globally. Continuing a history of innovation spanning more than 130 years, ABB today is writing the future of industrial digitalization with two clear value propositions: bringing electricity from any power plant to any plug and automating industries from natural resources to finished products. As title partner of Formula E, the fully electric international FIA motor-sport class, ABB is pushing the boundaries of e-mobility to contribute to a sustainable future. ABB operates in more than 100 countries with about 135,000 employees. www.abb.com

Share this article

Facebook LinkedIn Twitter