Global site

ABB's website uses cookies. By staying here you are agreeing to our use of cookies. Learn more

Power and automation solutions for Al Nasr Full Field Development Project

Back to Case studies page

Improved safety and reliability

The Abu Dhabi Marine Operating Company (ADMA OPCO) is developing a new oilfield in the Arabian Gulf. The Al Nasr field is located about 130 km off the coast of the United Arab Emirates, close to the same operator’s long-established Umm Shaif field.

ABB, has received orders from Hyundai Heavy Industries for electrical and telecommunication systems. It enables Hyundai Heavy Industries to fulfill its obligations to Abu Dhabi Marine Operating Co. under the contract for EPC Work of Nasr Full Field Development Project (Package 2).


The solution provided consists of power management, power-from-shore and telecom systems which are interconnected to ensure the highest levels of efficiency, reliability and safety. ABB has pioneered and proven the use of power-from-shore for energy platforms to help energy companies reduce emissions, ease operations and improve working conditions by lowering noise levels. The facilities covered by the referred contract will be powered by a 132 kilovolt (kV) AC subsea ring cable from Das Island, about 160 kilometers west of Abu Dhabi.
 

The power management system is based on ABB’s System 800xA Extended Automation control system, which integrates the network of transformers and switchgears and enables operators to control this vast electrical installation in a safe and consistent manner. It includes an intelligent asset management system for predictive maintenance of equipment, reducing operating costs and extending its service life.

ABB will supply 28 bays of compact 132 kV GIS for one onshore and two offshore platform installations as well as medium voltage products including 33 kV gas-insulated switchgear and 11 kV and 6.6 kV air-insulated switchgear. ABB pioneered high-voltage GIS in the mid-1960s and has a global installed base of more than 23,000 bays. Its product portfolio covers voltage levels from 72.5 kV to 1,200 kV.

Additionally, ABB will supply multiple types of transformers, shunt reactors and associated equipment ranging from 500 kVA to 100 MVA, minimizing losses through the lifecycle and lowering environmental impact. The transformers and reactors are suited for hazardous and challenging environments.

ABB will also provide a complete and fully integrated telecommunication system to the Al Nasr super complex for internal and external communication and field security. Key products are computer networks, electronic personnel tracking, a camera system, radar, public address and general alarm systems, access control, a telephone system, radios and a transmission system between platforms.

The project will be executed by ABB’s engineering services and project management team in Norway, with equipment manufactured by ABB in the Czech Republic, Finland, Germany and Norway. Delivery is scheduled for the third quarter of 2016.

ABB has supported the Al Nasr Full Field Development Project from the concept stage, through front-end engineering and design and now the construction phase. The scope of supply includes design, engineering, supply, installation and commissioning.

Main data

 Customer: 

Hyundai Heavy Industries Co. Ltd.

 Site:  Al Nasr offshore Abu Dhabi, UAE
Customer need: 

- Developing new offshore fields
- Reducing CO2 emissions
- Reducing operational expenditures
- Advanced predictive maintenance 
- Fully integrated telecommunication solutions     

Scope: 

132kV & 33kV GIS Switchgear
11kV & 6.6kV AIS Switchgear
LV Switchgear & Motor Control Centre
Power Transformers
Shunt Reactors
Electrical Control and Monitoring System
Power Management System
Asset Management System
Fully integrated Telecommunication Systems

Application: 

Power from shore
Power Management
Asset Management
Telecommunication

Customer benefits:

- Seamless integration
​- High reliability
- Reduced CO2 emissions
- Reduce maintenance cost 
- Minimize lifecycle cost
- World class project execution

Commissioning year: 2018

Links and downloads