Global site

ABB's website uses cookies. By staying here you are agreeing to our use of cookies. Learn more

Production of EI Merk oil and gas field in Algerian desert

Creating an industrial complex complete with 700 km of pipeline

The  El Merk oil and gas field in Algeria is located in the southern desert, 1,000 kilometers from the coast. It is being exploited by a consortium of six oil companies and managed by two of them: Anadarko and the Algerian state-owned producer Sonatrach, which together form the Groupement Berkine joint venture.

The project, which achieved its first oil in March 2013, is expected to reach a peak daily output of about 160,000 barrels of crude and condensate, and 600 million cubic feet of propane and butane.

An ABB-led consortium has fullfilled a $650 million contract to design and install much of the infrastructure for El Merk. As well as the power supply and the industrial plant required to lift and process the oil and gas, ABB is supplied 719 kilometers of pipeline and the production and collection flowlines for some 120 wells.

The pipelines, which will be fitted with almost 10,000 manual valves, connect the wells with field gathering stations, and link the stations with the central processing plant where the mixed gas and liquid will be separated and treated.

The pipelines are being laid with the help of ABB’s geographic information system, which surveys possible problems along pipeline corridors, such as changes in elevation and the angle of dune slopes and so on. It automatically generates the information needed to lay the pipelines in the field, and it also supports the pipeline open data standard model, the most widely used in the industry. ABB estimates that the use of this resource will cut 12 months from the construction time.

Main data

Customer:  Groupement Berkine 
Site:  EI Merk oil and gas field in southern Algeria
Customer need:  Field infrastructure for major industrial development in desert are with no pre-existing services

Design, manufacture and installation of a wide range of power, instrumentation, industrial, telecoms, together with related management and maintenance services

Design, procurement, transportation, construction, commissioning and startup of ten field gathering stations, six gas distribution manifolds, complete material supply for 120 wells as well as the hooking up of the first 80 for production, 719 km of pipelines and process piping across all four fields of block 208

Application:  Oil and gas production and transportation
Customer benefits:  Development of one of country's biggest oil and gas reservoirs
Commissioning year:  2014

Links and downloads