ABB's website uses cookies. By staying here you are agreeing to our use of cookies. Learn more


HVDC Light technology secures power supply and grid reliability to Finnish archipelago.

Kraftnät Åland AB is responsible for electricity transmission in the Åland Islands, an autonomous Finnish province situated at the entrance of the Gulf of Bothnia in the Baltic Sea. Kraftnät awarded ABB a contract to supply a turnkey, 100 MW  ±80 kV HVDC Light transmission link to ensure security of the energy supply on the main island of Åland, where most of the population lives, and allow more renewables into the energy mix.

Åland presently receives 70 percent of its power via subsea AC cables from Sweden, in addition to some locally produced renewable generation. The existing fossil fuel powered back-up system will be closed once the new HVDC Light link is in operation, saving CO2 emissions.

The HVDC Light system incorporates special features such as active AC voltage support providing greater network stability and the unique ‘Black-start’ capability, which provides faster grid restoration in the event of a blackout.

With the ‘Black Start’ feature restoration time can be reduced to fractions of a second under operational conditions. This functionality when incorporated with ABB’s HVDC Light® technology, performs an intelligent and controlled injection of electricity into the grid to quickly re-energize the system.  Even when the link is not in active operation, the black-start system can restore power in under five minutes - many times faster than in the absence of this feature. 

The ÅL-link is grid enabled, i.e. prepared for a multi-terminal configuration, which allows for additional in-feed from stations, such as future wind power plants.

ABB will deliver two converter stations, one situated in Ytterby, Åland and the other in Nådendal, Finland, and two 80 kV submarine cables, each 158 km long.

Main data

Commissioning year: 2015
Power rating: 100 MW
No. of poles: 2
AC voltage: 110 kV at both ends
DC voltage: ±80 kV
Length of DC submarine cable route: 158 km
Main reason for choosing HVDC: Length of sea crossing
Asynchronous networks
Reliable backup power
Application: Interconnecting grids

Related links