Global site

ABB's website uses cookies. By staying here you are agreeing to our use of cookies. Learn more

History

ABB is the product of many acquisitions and mergers, but primarily the 1988 coming together of ASEA and BBC, formerly known as Brown Boveri, two of the proudest and best known names in European electrical engineering history.

Milestones

2017

ABB launches ABB Ability™ , its our unified, cross-industry digital offering — extending from device to edge to cloud — with devices, systems, solutions, services and a platform that enable our customers to know more, do more, do better, together

2014

ABB unveils the future of human-robot collaboration: YuMi®. The innovative human-friendly dual arm robot with breakthrough functionality unlocks vast global additional automation potential in industry.

2012

ABB successfully designs and develops a hybrid DC breaker suitable for the creation of large inter-regional DC grids. This breakthrough solves a technical challenge that has been left unresolved for over a hundred years and was perhaps one of the main influencers in the 'war of currents'.

2008

NorNed, the longest submarine HVDC cable in the world at 580 km, links the power networks of Norway and the Netherlands with a transmission capacity of 700 MW.

2011

ABB developed an awarding winning technology for the comprehensive recycling of contaminated sulphur hexafluoride (SF6 ) gas. The new technology was implemented at a dedicated gas recycling centre in Australia. The purity of recycled gas enables it to be reused again and again.

2005

ABB delivers electricity through a DC (direct current) link originating 70 km away on land to a gas platform in the North Sea, helping avoid annual emissions of 230,000 tons of CO2 and 230 tons of NOX.

2004

ABB launches its Extended Automation System 800xA providing a process automation system that has since been installed at thousands of medium to large process plants in the Oil & Gas, Chemical, Pulp & Paper, Metals, Mining and Life Sciences industries delivering continuous productivity improvements.

2002

ABB links the AC (alternating current) networks of South Australia and Victoria with the world’s longest underground transmission, a 177 km HVDC Light cable with a capacity of 220 MW. ABB also linked Conneticut and Long Island with the world’s first extruded HVDC submarine transmission, a 40 km HVDC Light cable with a power rating of 330 MW.

2000

ABB delivers world’s first commercial high-voltage shore-to-ship electric power, helping reduce greenhouse gas emissions from ships berthed at the Swedish port of Gothenburg.

1988

ASEA and BBC merge to form the new company, with headquarters in Zurich, Switzerland. The new group, which started operations on Jan. 5, 1988, had revenues of $17 billion and employed 160,000 people around the world.

ASEA

BBC

1986

ASEA employs 71,000 people and reported revenues of $6.8 billion and income after financial items of $370 million.

1986

BBC employs 97,000 people and reported revenues of $8.5 billion and an income after financial items of $132 million.

1971

BBC builds the most powerful transformer in the world at 1,300 MVA (megavolt ampere)

1978

ASEA launches one of the first industrial robots.

1965

BBC builds the first 110 kV GIS (gas-insulated switchgear) allowing circuit breakers to operate safely in a confined space.

1969

BBC develops the first gearless cement drive in the world.

1954

ASEA installs the world’s first HVDC transmission line, providing 20 MW, 100 kV to the Isle of Gotland over a distance of 96 km.

1957

The first MBB motor is produced at ASEA's Tottenham factory in Victoria, Australia

1963

ASEA achieves a major technological breakthrough with the introduction of an improved thyristor able to handle substantially more electrical current than existing devices.

1953

The first data transmission at carrier frequency is performed by BBC over a 735 kV high-voltage line to the power station control unit.

1954

ASEA receives an order for 2 x 80MW generators for the Snowy Mountains Hydro Electric Scheme (an order for two additional 80MW generators is received a year later) in New South Wales, Australia

1952

ASEA designs and installs the first 400 kV AC cable – a 70 m low pressure oil-filled (LPOF) cable connecting an underground power station (built to withstand an atomic bomb) to the Swedish grid.

1953

ASEA is the first company in the world to manufacture synthetic diamonds.

1942

ASEA builds the world's first 120 MVA, 220 kV transformer in the Stockholm Elverks Värtanstation

1943

BBC builds the first 110 kV high-speed air blast circuit breaker.

1933

BBC obtains the patent for turbine rotors constructed from individual steel disks that are welded together.

1938

The first turbo-alternator to be installed in Melbourne, Australia is order by the Melbourne City Council from ASEA Electric.

1939

BBC builds the first combustion gas turbine for generating electricity.

1901

BBC builds the first steam turbine in Europe.

1932

ASEA builds the world's largest self-cooling transformer rated at 2,500 kVA (kilovolt ampere).

1893

ASEA builds the first three-phase transmission system in Sweden

1893

Brown Boveri supplies Europe’s first large-scale combined heat and power plant producing alternating current.

1890

Elektriska Aktiebolaget merges with Wenströms & Granströms Elektriska Kraftbolag to form Allmänna Svenska Elektriska Aktiebolaget, later shortened to ASEA.

1891

Charles E. L. Brown and Walter Boveri establish Brown, Boveri & Cie in Baden, Switzerland. Shortly afterward, Brown, Boveri is the first company to transmit high-voltage power.

1889

Jonas Wenström invents the three phase system for generators, transformers and motors.

1883

Ludvig Fredholm establishes Elektriska Aktiebolaget in Stockholm as manufacturers of electrical lighting and generators.