Global site

ABB's website uses cookies. By staying here you are agreeing to our use of cookies. Learn more

ABB Bulgaria EOOD - Petrich Branch

Production unit

ABB’s production unit in Petrich is built in 1996 on total area of 5.000 sqm and the factory has expanded ever since. The city is located in Southwestern Bulgaria, near by the main exit road for Greece, 17 km away from the Greek border and 20 km away from Macedonia. The total population of Petrich is of approximately 30 000 people.

The main activity of the ABB production unit in Petrich focuses on acting as an outsourcing producer for electro-mechanical assemblies, including welding / winding / pressing / assembling of sub-assemblies for low voltage control products and DIN rail mounted products. Customers of the factory are ABB companies in Western Europe, such as Germany, Switzerland, Czech Republic etc.

The capacity of the factory allows working on two shifts and currently ABB is employing around 300 employees. 

The quality service, competitive prices and timely delivery of products according to a high technological standard, ensure to our customers a decisive advantage over their competitors.

Contacts

ABB Bulgaria EOOD - Petrich branch
1, Varna str., 2850 Petrich
Telephone:  +359 745 594 18 ; Fax:  +359 745 594 28
E-mail: abb.petrich-branch@bg.abb.com


See larger map