Global site

ABB's website uses cookies. By staying here you are agreeing to our use of cookies. Learn more

ABB Jiangjin Turbo Systems Co., Ltd

ABB Jiangjin Turbo Systems Co., Ltd

ABB Jiangjin Turbo Systems Co., Ltd was founded in 2006 as a joint venture of ABB China and CSIC-Chongqing Jiangjin Turbo & Charger Machinery Co., Ltd. It has grown into the second largest manufacturing location and the sole production base of small- to medium-sized turbochargers for low-speed diesel engines of ABB Turbocharging, and is an important pillar in the global setup.

ABB Turbocharging is at the helm of the global industry in the manufacture and maintenance of turbochargers for 500 kW to 80+ MW diesel and gas engines. Turbochargers provide 75% of an engine’s power and can contribute to reducing fuel consumption by up to 10%, depending on the application and operating environment. Our leading-edge technology and innovation enables our customers to perform better and produce fewer emissions, even in the toughest terrains. Approximately 200,000 ABB turbochargers are in operation across the globe on ships, power stations, gen-sets, diesel locomotives and large, off-highway vehicles.

Adhering to the “In China, for China and the World” strategies, ABB Jiangjin Turbo Systems have been supporting China to upgrade into a manufacturing power with innovative technologies and local service under the guidance of the market-oriented and customer-centered principles. The company have successfully localized the production of the latest generation of A100 and A200 series for marine engines, TPR-series with Variable Turbine Geometry technology customized for the local locomotive market as well as CR-series customized for the China River Shipping market.

With the manufacturing center located in Degan Industrial Zone, ABB Jiangjin Turbo Systems have well established a local service network, by successively opening up service stations in Hong Kong, Guangzhou, Shanghai, Tianjin, Dalian and Qingdao. All the service stations are integral to the global service network and sharing the same database via scientific and intelligent management of information. Trained engineers will provide customers with 24/7 a wide service portfolio that guarantees Original Parts and Original Service.

You can view this page in:

  • EN

Offerings
Milestones
Contact us

2017

  • ABB turbochargers are powering the main engines and auxiliary engines of the largest containership ever built in China, a 20,000 TEU vessel named COSCO Shipping Taurus, launched in June 2017

2016

  • ABB first locally produced A100-L for export

2015

  • China’s largest semi-submersible vessel, Guang Hua Kou, has ABB turbochargers onboard

2014

  • The company starts to produce ABB TPR56, a model developed for China rail market
  • China Mobile Cloud Corporations’cloud computing data centers have ABB turbochargers onboard
  • The world’s largest container ship in 2015 , the CSCL Globe, has green power provided by ABB turbochargers

2013

  • China’s only expedition vessel for polar research, the Xue Long, has ABB turbochargers fitted on the main engine

2012

  • The world’s largest turbocharger, ABB TPL91-L, is onboard COSCO’s 13,800 TEU container ships

2011

  • The company manufactures its 10,000th turbocharger
  • China’s first deep water crane ship, the Offshore Oil 201, has ABB turbochargers on board
  • The company manufactures the first and most efficient A100-L turbocharger for low-speed diesel engine

2010

  • The largest thermal power plant in Tibet, Lhasa Dungkar Thermal Power Plant, has its turbochargers successfully upgraded, improving power output by 25%

2009

  • The 6th service station is opened in Qingdao
  • First shipment of locally produced TPS turbochargers

2008

  • China’s first 8K90MC low-speed diesel engine is successfully equipped with ABB TPL 85-L

2007

  • China’s first capsize bulk carrier is equipped with ABB turbochargers

2006

  • ABB Jiangjin Turbo Systems Co. Ltd officially goes into operation

Company President: Allan Wang
Communications Contact: Dolphy Liu
Tel: +86 23 4784 7888
Fax: +86 23 4784 7999

Address:
Dongjiang Road 23, Degan Industrial Zone, Jiangjin District, Chongqing, China. 402284

  • Contact us

    Submit your inquiry and we will contact you

    Contact us