容量——随着新的需求不断扩张

满足不断增长的全球电力需求意味着在未来二十年里每周都要新增一座十亿瓦特(1 GW)的电站以及配套基础设施。必须利用有效的环保技术,并以最经济的方式实现此目标。其中,减少二氧化碳排放尤为重要。

满足日益增长的电力需求

满足不断增长的全球电力需求意味着在未来二十年里每周都要新增一座十亿瓦特(1 GW)的电站以及配套基础设施。国际能源署(IEA)预计从现在到2030年,全球需要在电网基础设施方面投资大约6万亿美元以满足不断增长的电力需求。预计大部分新增投资将用于亚洲的新型输电和配电系统建设,不过美国和欧洲老化的电力系统同样需要新的投资来进行更新换代。为确保电网的容量尽可能得到有效利用,除了将备用容量(用来平衡需求与供应波动)最小化,还需要具有高容量线路的大型跨国电网。将建成更多旨在满足本地需求的小规模电站,支持中心电站的工作。

以纯电动车辆替代传统的机动车辆的趋势正在加速,需要足够的配套充电设施给潜在的数以百万计的汽车电池充电。这不但增加了总的用电量需求,同时也给电力系统提出了更高的要求。为电动汽车充电的基础设施将成为未来电力系统必不可少的一部分。关于需要充电设施的电动汽车的数量,已经进行了很多预测。据波士顿咨询公司以及其他机构预计,到2020年,在用的电动汽车数量将达到四千万辆。大部分当前在用的低压系统不适合用于为电动车辆充电,因此需要新建基础设施满足快速和慢速充电需求。

可靠性

Providing high-quality electrical energy whenever it is needed

效率

Increasing the efficiency of power generation and reducing losses in transmission, distribution and consumption of electrical energy

可持续性

Ensuring the effective integration of renewable power generation

Select region / language