Venue for World Control Tour in Singapore

May 27 and 28, 2014 in Marina Bay Sands

Marina Bay Sands Expo & Convention Center

Melati Ballroom, Level 4
Singapore

 

Sands Expo and Convention Centre

Located in the heart of Singapore’s city centre, a mere 20-minute taxi ride
from Changi Airport and walking distance to the Central Business District –
they all add up to strategically position Marina Bay Sands as a compelling
MICE venue unlike anywhere in the world.

Travel by taxi

Sands Expo & Convention Centre
(Instruct the taxi driver to alight at the convention centre)
Marina Bay Sands
10 Bayfront Ave
Singapore 018956
Phone: +65 6688 3000
Email: sales@marinabaysands.com

Other transportation

MRT (Train)
Sands Expo & Convention Centre is linked directly to the Bayfront MRT
station (Circle Line).
Map of MRT network 
 
Bus
Sands Expo & Convention Centre can be reached via the following buses:
97/97E, 106, 133, 502/502A, 518/518A, NR1 and NR6

Driving to MBS

Parking Coupon for Conference Participants For conference participants who park at MBS, a limited number of complimentary parking coupons will be provided. The coupons will be provided on a first-come-first- served basis to participants who request for them at the registration desk as they register to attend the conference.    Participants who are not able to obtain any of the complimentary car parking
coupons can purchase coupons at the special rate of S$6.00 per day, from the
registration desk.
 
Location of Marina Bay Sands
292x195-3x3-6 
Select region / language