Freelance: Glinojeck Sugar Plant Modernization

PRO-CONTROL started cooperation with Glinojeck Sugar Plant in 1998 with modernization of diffusion, evaporators, raw juice filtration and boilers. The existing pneumatic system was replaced by Freelance.

ABB system in Glinojeck Sugar Plant

After 12 years of almost continuous modernization of the plant in Glinojeck supported by ABB Freelance systems at all facilities except turbine control. Engineers and operators were given a modern and efficient solution, which consists of:
– 4 Engineer Stations
– 18 Operator Stations
– 28 Process Stations


Glinojeck Sugar Plant has reached and exceed assumed capacity goals in 2005 (12,200 tons / day) – up to 70%.

MES Plans

Water usage monitoring – PRO-CONTROL has implemented pilot system for data collecting and analyzing. PGIM is a dedicated solution for production media monitoring, that is necessary in the modern production management. Pilot implementation has helped to identify important sources of cost reduction (water/steam leaks etc.) 

Results

ABB Freelance system that was implemented by PROCONTROL together with huge technological enlargement has contributed to increase the reliability and clarity of sugar production, which allowed to achieve ambitious business goal. Glinojeck Sugar Plant has reached and exceed assumed capacity goals in 2005 (12,200 tons / day) – up to 70%. Of course next year assumed profitability of the production has been reached.


Scalable Freelance system allows for phased development and system enlargement in the future.

It was possible thanks to the substantial downtime reduction due to new control system and electrical equipment and easy access to all critical information. Reliability and possibility of rapid response and correction of process parameters. The system’s flexibility, size and investment matched with sugar plant process requirements. 

Scalable Freelance system allows for phased development and system enlargement in the future. Additionally the coherence of the system allows for easy implementation of PGIM. 12 years of continuous cooperation between ABB, PROCONTROL and Customer seems to be the best recommendation of the technical solution and business partnership.

PRO-CONTROL Ltd.

The company was established in 1991 and now is one of the leading polish engineering companies in Industrial Automation & Industrial Information Technologies. Company specializes in PLC/DCS applications, industrial software (MES), robotics and vision systems. Pro-Control offers complex services starting from automation audits by electrical design, programming, cabinets and on-site assembling, deliveries ending on the installation maintenance.

Pro-Control company services various industries, among them food & beverage, pharmaceutical, chemical, heavy industries, energetics, gas & oil, automotive.

Sugar Plant Glinojeck

Glinojeck Sugar Plant was constructed in late 70’s. In 1997 BSO Poland acquired a controlling interest in Sugar Factory Glinojeck SA, and followed that by under-writing Glinojeck’s share acquisition of two neighbouring factories. Glinojeck SA become the largest sugar factory in Poland in terms in its daily beet slice and annual production, which in year 2002 was above 100,000 tons of sugar.

BSO has moved production and beet quotes from 4 different sugar plants and concentrated this in Glinojeck Sugar Plant. New production strategy tied to the need for replacement of old, treacherous control system and development of production technology for increasing capacity and production efectiveness (7,5 k to 12 k tons/day).
  • お問い合わせ

    ご質問内容などをご入力の上、お送りください。 担当者より折り返しご連絡いたします。

    お問い合わせ
Select region / language