ABB Ability™ InSite Energy Pro

Elevating energy efficiency, from ground to cloud

In today's increasingly complex energy landscape, characterized by the integration of renewables and electrical loads like heat pumps and EV chargers, managing energy efficiently has become more challenging, especially for those overseeing multiple properties. To address these challenges, ABB Ability™ InSite Energy Pro provides a comprehensive cloud-based platform for intuitive, multi-site energy management.


With customizable dashboards that provide actionable insights, users can benchmark performance and identify energy-saving opportunities, while real-time monitoring and automated reporting enhance energy efficiency and support compliance with sustainability regulations.

Select Language
  • English
  • Deutsch
  • Ελληνικά
  • français
  • italiano
  • Nederlands
  • polski
  • svenska
  • български
commercial application

Let's get in touch!

Contact us

Elevating energy efficiency, from ground to cloud

InSite Energy Pro Compact
Easy implementation and retrofit
  • Reduce complexity, costs and space with only one control unit as the main gateway
  • Easy retrofit and upgrade of existing installation at any time, minimizing impact on building operations
  • Enable integration and connection to other 3rd party systems, using the data from the cloud to enrich the electrical data ecosystem
InSite Energy Pro Multisite
Intuitive energy management
  • User-friendly interface with multi-location view, property status indicators, and comprehensive property details
  • Customizable dashboards with a broad range of widgets for tailored views according to each application's needs
Decision-making
Accelerate decision-making
  • Remote monitoring of real time energy data, KPI overview, and alerts to keep always informed and allow proactive behavior
  • Manual control of selected loads to quickly act in case of any critical situation
  • Benchmark analytics allow for comparisons between different devices, groups or properties to identify areas of improvement 
InSite Energy Pro Reporting
Reporting and transparency of energy data
  • Comprehensive reports that aggregate different data sources to show energy usage and cost distribution across different sites
  • Makes energy data more accessible and transparent, keeping key stakeholders up-to-date about the overall performance and KPIs
  • Supports compliance with energy efficiency regulations (e.g. ISO 50001)

Explore the Cloud

System architecture

The InSite energy management system’s control unit, SCU200, manages energy across various devices, such as breakers, meters, and Electric Vehicle (EV) chargers and acts as a central gateway.

When connected with ABB Ability™ InSite Energy Pro, users can obtain a holistic view of their energy ecosystem, facilitating load management, performance optimization, and cost reduction.

Key functionalities include:
  • Customizable energy dashboards
  • Multi-location property overview
  • Asset management to keep track of connected devices
  • Manual control functionalities
  • Benchmark analysis
  • Alarm set-up to be notified in case of critical situations
  • Export reports to share with stakeholders and authorities

Main applications


commercial application
Commercial buildings

Various businesses operate across multiple locations, each with unique energy performance and management needs. Without the right tools, navigating these complexities can be challenging.

Implementing a comprehensive energy management solution can streamline operations, enhance energy efficiency, and provide actionable insights, ultimately optimizing energy use and supporting sustainability goals while reducing costs.

 


InSite Energy Pro_multi-dwelling
Multi-dwelling units
Multi-dwelling units present a variety of diverse energy management needs. Property owners and community managers require a comprehensive approach to oversee energy usage across the entire complex, while tenants seek ways to stay informed and enhance their energy management practices.

With a centralized platform like ABB Ability™ InSite Energy Pro, stakeholders can accelerate informed decision-making based on real-time energy data, insights and benchmark analytics, enabling effective energy management and operational efficiency.

FAQ


Which gateways are able to connect to InSite Energy Pro?

The main control unit of ABB's InSite energy management system, SCU200, is the only gateway that can connect to InSite Energy Pro. The SCU100 control unit is not able to connect to InSite Energy Pro.

How does the device commissioning process work? Is a separate tool needed?

No separate tool or software is needed. The commissioning is done on the SCU200 web server as it is traditionally done. Once the cloud commissioning process starts, the devices connected to the web server will be automatically recognized in the cloud.


Why do I need an authenticator app?

The authenticator app allows us to verify your credentials and adhere to cybersecurity standards. For iOS users, an authenticator app can be downloaded from the App Store. For Android users, it can be downloaded from the Google Play Store.


What type of devices can be configured or visualized in InSite Energy Pro?

All the devices that can be technically connected to the SCU200 (according to its communication protocols) can be configured and visualized in InSite Energy Pro. The available widgets will allow different types of visualizations according to the nature of each device. 

Let's get in touch!

Select region / language