Overview

With ABB-AccessControl you can handle complex access management easily and user-friendly. Via the Smart Access Point the system can be used as a stand-alone solution or as part of a building system scalable for every requirement. ABB-AccessControl transmits data highly encrypted. Access is possible via the MyBuildings portal powered by ABB Ability via remote control. ABB-AccessControl can be combined with ABB-Welcome IP via the Smart Access Point.

One-family house

In "ABB-AccessControl" system the main entrance in a one-family house is equipped with an "Electronic cylinder lock". Aside from the "Electronic cylinder lock" a "Smart Access Point Pro" is necessary for the user management.

 

Multifamily house with one floor

In "ABB-AccessControl" system the main entrance and the entrances to the apartments in a multifamily house are equipped with "Electronic cylinder lock". Aside from the "Electronic cylinder lock" a "Smart Access Point Pro" is necessary for the user management.

 

Multifamily house with several floors

In "ABB-AccessControl" system the main entrance and the entrances to the apartments in a multifamily house are equipped with "Electronic cylinder lock" Aside from the "Electronic cylinder lock" a "Smart Access Point Pro" is necessary for the user management. The ceiling of the floor greatly reduces the transmission range of the radio signals. That is why the additional use of an "RF/IP Gateway" is required for the distribution of data for each additional floor.

 

Multifamily house with a medical practice

In "ABB-AccessControl" system the main entrance and the entrances to the apartments in a multifamily house are equipped with "Electronic cylinder lock". The building contains a medical practice. The archive in the basement should also be equipped with an "Electronic cylinder lock" for the medical practice. There is no radio connection to this room.

Aside from the "Electronic cylinder lock" a "Smart Access Point Pro" is necessary for the user management.The ceiling of the floor greatly reduces the transmission range of the radio signals. That is why the additional use of an "RF/IP Gateway" is required for the distribution of data for each additional floor.

 

Residential building with a longer floor

In "ABB-AccessControl" system the main entrance and the entrances to the apartments in a single-floor residential building are equipped with "Electronic cylinder lock".

Aside from the "Electronic cylinder lock" a "Smart Access Point Pro" is necessary for the user management. Fire walls greatly reduce the transmission range of the radio signals. That is why the additional use of an "RF/IP Gateway" is required for the distribution of data for each area between the fire walls.

 

Residential buildings with several floors

In "ABB-AccessControl" system the main entrance and the entrances to the apartments in a multi-floor residential building are equipped with "Electronic cylinder lock".

Aside from the "Electronic cylinder lock" a "Smart Access Point Pro" is necessary for the user management. The ceiling of the floor greatly reduces the transmission range of the radio signals. That is why the additional use of an "RF/IP Gateway" is required for the distribution of data for each additional floor.

 

Further system information

Select region / language