Advantages

advantages_header_intrusion-alarm-systems

Arm the security system with only one touch. When you leave the building you can trigger a full scene: Arming the security system, switching of the light, setting the heating and air-conditioning system to a defined absence state and, depending on the time of day, closing the shutters..

Highest safety & security in case of an alarm

If an alarm is triggered, lights can be switched on and shutters can be opened as an additional deterrent. Even when you’re at home, ABB solution can, for example, ensure the peripheral protection of your house and, in the event of an alarm, also switch on lights together with the siren and open the shutters.

Increased comfort and safety

By disarming the security system, the system switches the lights on in the entrance area and sets the heating to comfort mode. All the security sensors, such as those for water, gas, and smoke are active at all times. If there is an alarm, they control useful functions such as sockets, shutters and lights.

Being safe at home, even when the alarm system is not activated

Imagine the following: you are at home, some intruders may try to gain access at night or using unwatched entrances. The alarm system is switched off. You can activate the panic function by a press of a button: lights switch on, blinds roll up.

Further system information

Select region / language