A state of the art school

art_school_1183x353

The perfect learning environment with ABB i-bus® KNX building automation system

Zukowo school in Poland is one of the few public educational institutes in the country that has advanced building automation capabilities like this one.  To create the most productive and comfortable learning conditions, a school needs to have optimal lighting and temperature control.

Each room in the school is equipped with an automated air conditioning control system, enabling optimal conditions during classes according to the school timetable. Consequently, participation in class is greater. The following three temperature modes will be set in classrooms: comfort, holiday and anti-freeze. These modes will be activated depending on the classes scheduled and weather conditions.



school_292x146
convenient-control_292x146

Convenient control

The intelligent system, which is distinguished by its simplicity and reliability, will operate according to a specific school schedule. The school’s headmaster will be able to manage the entire system, though everyday functions will not require any additional control. During holidays, when there will be no pupils in the classrooms for a prolonged time, the heating will reduce the temperature automatically and can be switched to ‘Holiday’ mode.

Ventilation in the building, water heating temperature and the condition of fire dampers (smoke ventilation system) in air ducts are also controlled automatically. Moveable exterior shutters adapt to outdoor lighting conditions.



Harnessing a natural energy

Solar panels generating additional power, which are controlled by ABB string inverters, have been installed on the school’s roof. By converting sunlight into electricity, the school generates energy to satisfy its own needs.





School-solar-on-roof_292x146
School-sports-hall_292x146

Intelligent and energy efficient communal areas

All rooms and passageways feature the best quality presence detectors, which will activate the appropriate lighting upon detecting movement in the building, providing an energy efficient solution. When windows or doors are opened somewhere, the heating will switch off or the heat delivery from the central heating system will be reduced. The ABB i-bus® KNX system also controls the lights in the sports hall. The outside lighting of the school’s grounds and the facade is controlled by an astronomical clock, which connects via the KNX system and ‘operates’ the lighting.





Discover more

  • Contact us

    Submit your inquiry and we will contact you

    Contact us
Select region / language