Source Ground Return with SACE Emax 2

All the advantages for consultants


The customers

SEI S.r.l. was founded in 2005 and in few years has become a leading company as manufacturer of LV switchgear. It is present  worldwide with high-quality products, which can be customized to meet the designing requirements of its customers.

The challenge

The project concerns a plant for crude oil delivery realized on behalf of an oil and gas company. The challenge was to provide complete and total protection against earth faults in any point of the plant, with the commitment of guaranteeing  selectivity between the MV and LV circuit-breakers to isolate only the area affected by the fault.

The ABB solution

Using the Ekip Hi-Touch trip unit and with no need of indirect multifunction relays, it has been possible to protect the plant by  managing two independent curves for the protection against earth faults (function G).
Thus, the function Source Ground Return is implemented, which guarantees protection against the earth faults, both on the  supply (restricted) as well as on the load side (unrestricted) of the circuit-breaker terminals, and protection for the connection  cable (from the transformer secondary winding to the circuit-breaker terminals).
The solution with SACE Emax 2 guarantees time selectivity for any earth fault on the load side of the LV circuit-breaker thanks  to such a quick trip time that the fault is eliminated before the MV circuit-breaker receives the opening command.
In case of a fault between the secondary winding of the transformer and the input terminals of the LV circuit-breaker,
Ekip Hi-Touch, through the Ekip Signalling module, will command the opening of the MV circuit-breaker.

Select region / language