2014 was a record breaking year for skyscraper construction
A recent report by the Council on Tall Buildings and Urban Habitat (CTBUH) revealed that 2014 was a record breaking year for skyscraper construction. Globally, 97 newly constructed buildings were at least 200m tall, with 11 of those obtaining a ‘Supertall’ classification of 300m or taller.
This construction growth has resulted in 13 new buildings entering the world’s top 100 tallest list in 2014, including the high profile One World Trade Center in New York. London in 2012, as well as hosting the Olympics, saw the completion of The Shard, Europe’s tallest building, and more recently in 2014 the completion of the Leadenhall Building (known locally as the Cheesegrater) which at 225m (738ft) is the 4th tallest building in the UK.
The automation of these buildings, like many others, plays an increasing role in providing the functionality throughout the structure for lighting, heating, data, security and emergency systems. With the amount of electrical wiring potentially running into the thousands of metres, ensuring that these vital power, lighting, communication and security arteries are protected and can continue to perform reliably and safely is essential to the success of a building’s operation.
Consideration of the necessary characteristics for cable conduit protection - such as enhanced low fire hazard properties for safety, or overbraiding for security and EMI shielding – is vital. Choosing a supplier with the experience, expertise, and tried and trusted track record for delivering leading-edge flexible conduit systems has never been more important. It’s why so many businesses come to Adaptaflex for cable protection.
We have an unrivalled range of flexible conduit and fitting systems for construction applications, including our proprietary Adaptalok ATS system - which features a quick to install, twin-shot one-piece conduit fitting rated to IP68. It’s designed to make conduit installation quicker, easier and – most importantly – more reliable. Adaptalok ATS is win/win, proven to save construction businesses time and money while also removing the risk of incorrect installation and any subsequent system downtime.
Office Buildings
Schools
Hospitals (EMC)
Retail Developments
Leisure Complexes/Sports Stadiums
Office Buildings
Schools
Hospitals (EMC)
Retail Developments
Leisure Complexes/Sports Stadiums