From The Lab: Ingress Protection (IP) Testing of Harnessflex Sealed Conduit Systems

In the first edition of our "From the Lab" series, we test Harnessflex NC Conduit and Sealed Fittings to IP69 (IEC BS EN 60529) standard


It is often said that an electrical system is only as reliable as the conduit and fittings used to protect the cables. With electrical wiring representing the heartbeat of any heavy automotive vehicle as it navigates treacherous terrain in demanding environments, it is critical that wiring is kept safe and secure in order to maintain vehicle productivity.

That said, it is not just during intensive applications where vehicle wiring needs to be protected, but also in day-to-day maintenance too. High pressure washing is a common way of keeping buses, trucks and other specialist vehicles clean and presentable, however without the right conduit system in place it can leave vehicle wiring vulnerable to damage.

With this in mind, we decided to test the resilience of our Harnessflex Sealed Conduit systems in our in-house Ingress Protection (IP) testing chamber. Through our IP testing chamber, we are able to replicate a variety of real world scenarios - from sprays that may come from light rain fall through to power water jets that come as a result of a vehicle being cleaned down. Based on how the system performs under the testing conditions, it is granted an IP rating which is used to classify the degree of protection provided by enclosures of electrical equipment.

To see how our Harnessflex Sealed Conduit systems protect vehicle wiring against close-range, high pressure, high temperature spray downs, we tested a sample under IPX9 to IEC BS EN 60529 conditions. This involved placing a roll of paper inside the system, spraying it from multiple angles as it rotated and seeing if any ingress occurred causing the paper to dampen. We are pleased to say that after testing seven different systems three times each inside the chamber, every time the paper remained dry and the IPX9 test was passed (see detailed results below).

This means that by installing a Harnessflex Sealed Conduit system, you can help ensure that vulnerable connectors are not exposed to the elements, impact of foreign bodies or jet washing. Offering IP69 protection, Harnessflex solid conduits with attached sealed fittings ensure the risk of any electrical failure is minimised, helping to keep critical wiring safe during any routine cleaning or wash down.
Select Language
  • English
  • français
IP69 testing
The sealed system samples were entered into the IP testing chamber as shown, with a roll of paper wrapped up inside the conduit to detect any leakage.
Pressure wash
These test results show how Harnessflex Sealed Conduit Systems can help protect critical electrical wiring in heavy automotive vehicles against the impacts of day-to-day pressure washing.

More information

Select region / language