Recommended tightening torque values for installation of PMA Fittings

Select Language
  • English
  • Deutsch
  • français
tightening torque values_1183

The tightening torque values quoted below should be considered as absolute maximum values which should not be exceeded.  They are based upon practical laboratory measurements under standard climatic conditions (23°C / 50% relative humidity). Climatic conditions during assembly and in the application, which may affect the component characteristics, should be considered.

Fact sheets about PMA recommended tightening torque values

Select region / language