UKCA
UK Conformity Assessed (UKCA) marking is a conformity mark that indicates conformity with the applicable requirements for products sold within Great Britain.
The UKCA marking became part of UK law at the end of the Brexit transition period, on 31 December 2020, with the coming into force of The Product Safety and Metrology etc. (Amendment etc.) (EU Exit) Regulations 2019. It has been mandatory since then, although, until 31 December 2024 (an extended deadline, which was previously 1 January 2022 then 31 December 2022), the CE mark is accepted as a valid alternative. The scope and procedures of the UKCA scheme will initially follow those for CE marking, but after 31 December 2020 the two schemes may diverge.
With the UKCA designation as well as the conformity explanation, PMA certifies the accordance of the relevant products with the requirements of the low voltage guideline.