PMA® Testing: DSC – Differential Scanning Calorimetry

Select Language
  • English
  • français

According to ISO 11357

The DSC method, as outlined in standards such as ISO 11357, specifies a technique for measuring the heat flow associated with thermal transitions in materials. This test is conducted using a differential scanning calorimeter, where a small sample is subjected to a controlled temperature program while compared to a reference. This method is essential for R&D in polymer engineering and material science, providing critical data on the thermal behavior, phase transitions, and processing characteristics of materials

 

Select region / language