The elegant Busch-iceLight® was developed on the basis of state-of-the-art LED technology. LEDs are superior to conventional incandescent or halogen lamps in many cases. Their service life amounts to up to 100,000 operating hours, which means less maintenance. LEDs emit hardly any heat, are insensitive to jolts, and do not have hollow bodies that can implode. In addition, they generate a pleasant, even light. They are extremely efficient since they consume only one-fifth of the current of conventional lamps. If the Busch-iceLight® were to be lit around the clock for 365 days, for example, the current price would be 30 cents at an average price of 23 cents per kilowatt hour. (When using the nightlight module.)