By pressing the emergency call button an alarm message is generated in the form of a continuous audible signal and a flashing signal light outside the toilet. The LED (relief light) integrated into the button indicates to the person needing help that her/his call has been recognized and that help is on the way. Pressing the stop pushbutton, which is preferably installed next to the WC door, acknowledges the alarm and the relief light as well as the acoustic and optical signal go out.
The call system can easily be extended by further signal buttons and remote signalling if required.
With Busch-Infoline® Busch-Jaeger has created a system that does justice to every requirement and can be ideally integrated in the switch ranges Busch-Duro 2000® SI/SI Linear, Reflex SI/SI Linear, Busch-axcent®, future® linear and solo®.
Main benefits
- By pressing the emergency call button an alarm message is generated in the form of a continuous audible signal and a flashing signal light outside the toilet
- The LED (relief light) integrated into the button indicates to the person needing help that her/his call has been recognized and that help is on the way
- Pressing the stop push-button, which is preferably installed next to the WC door, acknowledges the alarm and the relief light as well as the acoustic and optical signal go out
Main features
- The call system can easily be extended by further signal buttons and remote signalling if required
- Busch-Infoline® can be ideally integrated in the switch ranges Busch-Duro 2000® SI/SI Linear, Reflex SI/SI Linear, Busch-axcent®, future® linear and solo®
- Different versions of inserts and cover plates are available