Panic/emergency call message

Just to be on the safe side

panic-emergency_header_1183x353

The area of application for panic and emergency call messages is in social security offices and psychiatric care facilities in which the personnel must be protected against possible assaults.

When an alarm is triggered by the threatened person, the red or yellow signal light in the corridor over the entrance door of the corresponding room lights up permanently. In all other rooms fitted with the alarm control unit the call for help is indicated by means of a clocked audible signal and the red flashing light.

The alarm message can only be acknowledged or reset at the monitoring insert in the room of the threatened person.
With Busch-Infoline® Busch-Jaeger has created a system that does justice to every requirement and can be ideally integrated in the switch ranges Busch-Duro 2000® SI/SI Linear, Reflex SI/SI Linear, Busch-axcent®, future® linear and solo®.

Highlights

Select region / language