Busch-iceLight® – Wall module Ambience

Individual to suit your mood

led-wand

The walls make the dimensions of a room come alive. A special effect can be achieved by a light integrated into the wall. This is made possible with the variable design covers. High-quality inlays that fit the respective ambience are available for the Busch-iceLight® - wall module ambience. In eight different grids and décors.

 It also offers different light directions and three colour temperatures. Two models are available. With one or four light directions to the left, right, top, and bottom. This model can also be converted to five light directions. In this case, one LED also lights at the front. In this way a personal atmosphere is created. And lends light a many-facetted character. In the process, it fits perfectly in the Busch-Jaeger switch ranges. And thus expands the possibilities for design, lighting, orientation, and the provision of information.

LED technology and durability


The elegant Busch-iceLight® was developed on the basis of state-of-the-art LED technology. LEDs are superior to conventional incandescent or halogen lamps in many cases. Their service life amounts to up to 100,000 operating hours, which means less maintenance. LEDs emit hardly any heat, are insensitive to jolts, and do not have hollow bodies that can implode. In addition, they generate a pleasant, even light. They are extremely efficient since they consume only one-fifth the current of conventional lamps. If the Busch-iceLight® was lit around the clock for 365 days, for example, the current price would be 30 cents at an average price of 23 cents per kilowatt hour. (When using the nightlight module.)

One idea for more ideas


The illuminating effect of Busch-iceLight® can be easily multiplied within the room. Through arrangements and arrays. On wall or ceiling. The freedom of illumination knows no limits. From a plain series from wall to wall to geometrically complex patterns, everything is possible. Especially on large surfaces, spectacular stagings can be creatively implemented.

pl-led-wand-03

More than next to each other. With each other


Whether with socket outlets or light switches - the impression the Busch-iceLight® gives in its interaction is always positive. In each constellation the elegant reserve of the design always presents a pleasing appearance. With the surface and colour of the frame contrast or a visual uniformity can be given to an ensemble.

pl-led-wand-05

Visual nuances to suit personal taste


High-quality inlays that fit the respective ambience are available for Busch-iceLight®. In eight different grids and décors. Simple geometric patterns. Structures which remind one of crystals. Shapes inspired by nature.

pl-led-wand-02

Main benefits

  • The Busch-iceLight® LED lamp is adapted completely to the desires of the inhabitants or the specific room situation
  • Two models are available
    Model one: With one or four light directions to the left, right, top, and bottom
  • Two models are available
    Model two: With five light directions to the left, right, top, and bottom and one LED also lights at the front

Main features

  • The elegant Busch-iceLight® was developed on the basis of state-of-the-art LED technology
  • LEDs are superior to conventional incandescent or halogen lamps in many cases
  • Their service life amounts to up to 100,000 operating hours, which means less maintenance

Highlights

Select region / language