Busch-iceLight® – Wall module Orientation

Light with labels

led-orientierung

Whether for one's path or one's goal - orientation is necessary for both. This is especially so in a world that is getting ever more complex. And it should appeal at the very first glance. Because this enables people to move about safely on unfamiliar terrain. Especially in buildings with public traffic is clear communication important. Also as an identifying sign of high-quality architecture. And here Busch-iceLight® Orientation gladly takes the lead.

Conspicuous due to its modest style

Numerous pictograms are available for the Busch-iceLight® - Orientation.They have a bold and simple design, are easily understandable, and provide information reliably, night or day. This efficient LED light provides light in four directions - to the left, right, top, and bottom. It also lights towards the front so that the respective pictogram can be seen clearly. As a result, you always know what's going on in dark areas of the building. Currently 30 versions are available - for almost all requirements in the commercial or semi-public sector.

LED technology and durability

The elegant Busch-iceLight® was developed on the basis of state-of-the-art LED technology. LEDs are superior to conventional incandescent or halogen lamps in many cases. Their service life amounts to up to 100,000 operating hours, which means less maintenance. LEDs emit hardly any heat, are insensitive to jolts, and do not have hollow bodies that can implode. In addition, they generate a pleasant, even light. They are extremely efficient since they consume only one-fifth of the current of conventional lamps. If the Busch-iceLight® were to be lit around the clock for 365 days, for example, the current price would be 30 cents at an average price of 23 cents per kilowatt hour. (When using the nightlight module.)

Everything is clear, even in the dark


Busch-iceLight® - Orientation is never overlooked in the dark. For one, this efficient LED lamp lights outwardly in four light directions. It also lights towards the front so that the respective pictogram can be seen clearly. As a result, you always know what's going on in dark areas of the building.

pl-led-orientierung-02

Clear information


Numerous pictograms are available for the Busch-iceLight® - Orientation. They have a bold and simple design, are easy to understand, and provide information reliably, night or day.

pl-led-orientierung-03

Main benefits

  • Busch-iceLight® - Orientation is never overlooked in the dark
  • For one, this efficient LED lamp lights outwardly in four light directions
  • It also lights towards the front so that the respective pictogram can be seen clearly

Main features

  • Numerous pictograms are available for the Busch-iceLight® - Orientation
  • Currently 30 versions are available - for almost all requirements in the commercial or semi-public sector
  • The pictograms have a bold and simple design, are easy to understand, and provide information reliably, night or day

Highlights

Select region / language