Busch-Heat alarm detector ProfessionalLINE

Your lifesaver

rm-waerme-abb

The Busch-Heat alarm detector ProfessionalLINE is especially suited for rooms with a higher generation of steam or dust - such as a kitchen or attic.

Optimum protection with networking


A protective network for your safety. The best heat alarm over several floors in houses and apartments is useless if it cannot be heard. If it is too far away. To this we object: with smoke and heat detectors that are easy to network. They provide safety from the cellar to the roof. Whether wired or radio controlled: if one detector recognizes a danger, all installed devices alert the residents immediately - irrespective of where the smoke is located. This increases safety enormously, especially at night if not all rooms are being used.

A connection to external systems such as vibrating pillows for the blind or light signal devices for the deaf, but also to KNX is possible at all times via the Busch-Smoke alarm detector relay.

Also in case of radio controlled networking, each single alarm unit is directly connected with all the others. If this is not possible for structural reasons, the next detector retransmits the radio signal (repeater function). The triggering smoke or heat alarm differs from the other devices in the house by means of a flashing alarm light. It is a safe network for your protection, because thanks to the lithium batteries that are permanently installed in the radio control module and which have a service life of ten years, the full functionality is of the networked alarm units is assured even during a mains power failure.

pl-rm-rauch-01-abb

Main benefits

  • The Busch-Heat alarm detector ProfessionalLINE is especially suited for rooms with a higher generation of steam or dust - such as a kitchen or attic
  • As 10-year detector it cares for uninterrupted safety
  • The lithium batteries are permanently installed and cannot be removed for other purposes

Main features

  • It triggers an alarm from a temperature above 57° C
  • A temperature sensor measures the heat
  • It can also be networked via cable or optional radio module

Highlights

Select region / language