Busch-Timer® for lighting control

The perfect light at all times

timer-beleuchtung

Let the sun rise and set. Sunsets are known to be atmospheric. You can also use this pleasant light at home. To do so, combine a dimmer insert with a timer. You will thus be awakened automatically in the morning with a pleasant, dimmed light. When you get dressed, the light is always bright so that you have no problems choosing what to wear. In the evening, you can set the opposite effect. This is also idea for children's rooms. Atmospheric light for the bedtime story. Later the light continues to dim until it turns off entirely at night.

With the suitable flush-mounted inserts the comfort timer control element of the roller blind/Venetian blind control unit can be converted to a Busch-Timer® for lighting control. Then the timer operates, for example, in combination with a movement detector or a dimmer. When combined with LED dimmers, the Busch-Universal master dimmer or Busch-Memory touch-type controller, the brightness of the lighting can be adjusted for each turn-on time.

The KNX system offers comprehensive timing

Perhaps you want to wake up with music a bit later on the weekend? No problem. Venetian blinds go up, selected lights switch on, the radio begins to play and the heating system makes for a comfortable temperature at the right time – all at the time you set. In addition to settings by time and weekday, time periods can also be assigned with special settings. You can preset the special mood lighting you would like to enjoy for Christmas. Or under "Holiday", configure how the heating, lighting and other areas should be controlled during the holidays.

» Find out more about the KNX building system technology

Clever industry solution


We have another clever solution for commercial purposes. With the combination of a Busch-Universal master dimmer and a Busch-Timer® control element you can create economical and effective lighting concepts, such as for showcases, for example. Provide various showcases with pleasant light at different times of the day. This imbues your exhibition area with new dynamics. In the twilight hours, slowly increase the lighting of your exhibition area. Later, light only a part of the area and thus save money. You can also stage various scenes with slow dimming and brightening. Your creativity in getting customers attention knows no limits here.

pl-zu-beleuchtung-01

Highlights

  • Contact us

    Submit your inquiry and we will contact you

    Contact us
Select region / language