The China Energy Label scheme has been mandatory since 1.9.2008 and it was revised 2012.
To qualify for the China Energy Label, motors must meet the requirements specified in Chinese National Standard GB 18613-2012. The testing method under GB/T1032 is identical to IEC 60034-2-1 and the grades are in line with the classes in IEC 60034-30-1 (IE2/IE3/IE4).
In addition to energy efficiency requirements, low power motors are subject to CCC-certification.
ABB has a full range of LV motors meeting China Energy Label requirements.