ABB wins substation order to enhance Brazil’s power infrastructure and support soccer World Cup

Substation to boost transmission capacity and strengthen grid reliability in Rio de Janeiro

Zurich, Switzerland, September 4, 2013 - ABB, the leading power and automation technology group, has won an order worth around $30 million from Furnas Centrais Elétricas S.A. to construct a new indoor transmission substation in downtown Rio de Janeiro to power the renowned Maracanã soccer stadium and the adjacent neighborhood. The order was booked in the second quarter.

The Maracanã stadium was the world's largest when originally inaugurated in 1950, with space for around 200,000 spectators. It has been completely rebuilt for the forthcoming World Cup and, with a capacity of more than 75,000 people, is still the largest stadium in Brazil. It will host seven games in 2014 including the World Cup final.

Brazil is boosting its power capacity and enhancing its transmission and distribution infrastructure to ensure that its electricity grid can meet the needs of its expanding economy as well as the 2014 FIFA World Cup and the 2016 Olympic Games. These sporting events are likely to place huge additional demands on the grid as hundreds of thousands of fans and visitors descend on the 12 host cities.

Maracana Stadium / Image by Arthur Boppré
Maracana Stadium / Image by Arthur Boppré
center

"These compact substations will enable additional power supplies required during the forthcoming global sporting events being hosted by Brazil and will reinforce the transmission grid for the future," said Brice Koch, head of ABB's Power Systems division. "ABB has the range of technologies, the experience and the project management capabilities to support the country in its efforts to strengthen its power infrastructure."

ABB is to design, supply, install and commission a new indoor substation to replace a 40-year-old installation in Grajau, near the Maracanã stadium. Thanks to the compact footprint of the gas-insulated switchgear (GIS), the new higher-capacity facility can be built on the same plot of land as the existing substation.

At 63 kilo-amperes, the substation will have the highest short-circuit current interruption level of any GIS substation in Brazil. This rating refers to the maximum current that a circuit breaker is capable of interrupting to isolate a fault and protect the network. ABB will also install IEC-61850 substation automation, control and protection systems to enable local as well as remote control and monitoring.

Substations are key installations in the power grid that transform voltage levels and facilitate the safe and efficient transmission and distribution of electricity. They also include equipment that protects and controls the flow of electric power. ABB is the world's leading supplier of turnkey air-insulated, gas-insulated and hybrid substations with voltage levels up to 1,100 kilovolts.

Furnas is a subsidiary of Centrais Elétricas Brasileiras (Eletrobras), Brazil's largest power utility. It generates around 10 percent of Brazil's electricity and owns more than 20,000 kilometers of transmission lines as well as 54 substations.

ABB (www.abb.com) is a leader in power and automation technologies that enable utility and industry customers to improve their performance while lowering environmental impact. The ABB Group of companies operates in around 100 countries and employs about 145,000 people.

Links

Contact us

Downloads

Share this article

Facebook LinkedIn X WhatsApp