Fifty-one thousand solar panels are distributed over an area spanning 52 hectares to form five solar arrays, producing a total power output of 17.6 MW. These are the dimensions of the new solar park in Naro, in the Agrigento Province, one of the largest ground-mounted solar power systems in Italy. Manni Energy, specialized in the design, realization and management of power plants using renewable energy sources, and ABB, which together with its experience in the development of solar power solutions, provided 80 string inverters necessary for transforming and distributing the power produced to the main network, joined forces to realize this project successfully.
The award-winning PVS-175 string inverter was the perfect solution for this large ground-mounted distributed generation solar power plant. This high-performing model, characterized by high-power density in the string inverter segment, is capable of generating a maximum power output of 185 kW. With a maximum input voltage of 1500V the inverter allows the most recent solar panel technologies to be used, while its output voltage of 800V is optimized for distribution on the alternating current side. These features translate into substantial savings in terms of materials and installation times, in addition to logistics and maintenance costs.
To make the most of the solar array and further increase power production, each block of panels was fitted with mono-axial trackers that follow the sun’s movement from east to west. The utilization of 12 maximum power point trackers (MPPTs), special features of the PVS-175 inverters, made it possible to optimize the management of the 1700 installed trackers, achieving maximum power output under all conditions, with energy yields of 2,000 kWh per installed kilowatt.

Furthermore, the built-in digital communication platform makes the PVS-175 a highly advanced inverter for communications and control, offering effective and reliable remote monitoring of the five systems that make up the solar park. Inverter management through mobile devices and wi-fi connection with a guided procedure made configuration and commissioning especially quick. This is a fundamental feature, in particular when working with such large-scale systems.
The use of the PVS-175 inverter also yields benefits in terms of savings in time and costs, with its simple, rapid installation, thanks to an all-in-one design without any external components, modular construction with wiring box that can be removed from the power module, as well as providing plug and play connection. All of this comes with simple maintenance and easy direct access to internal components.
Innovative technology, high performance, flexibility and ease of installation make the ABB PVS-175 an excellent product, guaranteeing performance, reliability and economy, also for complex, large-scale systems.
ABB (ABBN: SIX Swiss Ex) is a pioneering technology leader with a comprehensive offering for digital industries. With a history of innovation spanning more than 130 years, ABB is today a leader in digital industries with four customer-focused, globally leading businesses: Electrification, Industrial Automation, Motion, and Robotics & Discrete Automation, supported by its common ABB Ability™ digital platform. ABB’s market leading Power Grids business will be divested to Hitachi in 2020. ABB operates in more than 100 countries with about 147,000 employees