ABB Motion at ONS 2022

Making a world of difference!

ABB is a major contributor for the energy transition facilitating a low-carbon and sustainable future.
Energy efficiency is not an if, it’s a must. It is a simple and impactful solution to mitigate climate change. It’s the low-hanging fruit we need to bridge our path to a future where all energy is clean energy.

There are approximately 300 million electric motors installed globally and they consume about 45% of the world's electricity. That can be significantely by introducing newest motor technology or controlling the motor operation with variable speed drives (VSD).

ABB Motions mission is to keep the world turning, while saving energy every day.  

Please explore our related offerings

Select region / language