I dream of a corruption-free India. A place where everyone works hard and gets what he deserves. A place that gives equal opportunity to everyone based on their knowledge and skills irrespective of their caste, colour, creed, or religion. A place where people don’t use other people around to get accomplishes their selfish motives.
But alas, India is far from the ideal place I imagine it to be. Everyone is so engrossed in earning money and enhancing their lifestyle that they don’t mind using corrupt ways to fulfill their dreams and ambitions. It is a common notion that those who work with honesty cannot reach anywhere. They hardly get any promotions and continue to earn meager salaries. On the other hand, those who seek bribes and use unfair means to accomplish their tasks climb up the ladder of success and make a better living.
It must be understood that although using corrupt ways is an easy way to make money in most cases, it does not make you happy. You may do well monetarily using such ill practices, but will you ever get peace of mind? No! You may find temporary happiness, but you will stay dissatisfied and unhappy in the long run.
Suppose each one of us must take a pledge to leave corrupt practices. This way, our life will improve, and our country will become much better.
Corruption Free India Essay 2 (300 words)
Introduction
India, a country that boasts of high values, morals, and traditions, is ironically faced with the problem of corruption. It is one of the various evil practices our country is fighting with. The whole system of the country is based on corruption at different levels.
The government of India should Set an Example.
India’s government and political parties are known for their corrupt ways. Instead of indulging in corrupt practices, they should rather work on overcoming the problem of corruption. They must set an example for the citizens and inspire them to work with honesty and dedication to reach their goals rather than using corrupt means.
Selection of Political Parties and Ministers
In India, anyone can stand for the elections and form a political party. The eligibility criterion does not include a person’s educational qualification. Some ministers haven’t even attended school and have completely zero knowledge about the political system. Some have a past criminal record. When such people govern the country, corruption is bound to happen.
A minimum educational qualification criterion must be set. Only those candidates who meet the educational criteria and have a clean record must be allowed to contest the elections. The candidates who win the elections must then be trained to handle their duties and responsibilities. An educated and well-trained person can certainly run the country better.
There must be a set protocol for everything, and the activities of the ministers must be monitored by a higher authority to see if it is being followed.
Conclusion
Though we want a corruption-free India, no one is ready to contribute to the cause. We are rather adding to it. To free our country from this evil practice, we must stand united and be honest in our endeavors.
Corruption Free India Essay 3 (400 words)
Introduction
Many countries around the world face the problem of corruption. India is one such country that is severely impacted by this problem. Corruption is the root cause of various other serious problems in our country.
Ways to Make India Corruption Free
We can fight corruption if we stand united and are determined to drive this evil away. Here are a few ways to rid the country of corruption:
Spread Education
Lack of education is one of the main reasons for the growing corruption. Many people belonging to the uneducated class use illegal and corrupt means to earn their livelihood. Spreading education can help in curbing this problem to a large extent. The government must make policies to ensure that every child in the country goes to school and secures education.
Give Strict Punishment
Strict laws must be made for people who indulge in corrupt practices such as taking and giving bribery, using illegal ways to expand their businesses, accumulating black money, etc. These people must be punished severely.
Conduct Sting Operations
The media and government should join hands to conduct sting operations to uncover corrupt people in different sectors. Such sting operations will not only uncover the corrupt people but will also discourage others from indulging in such practices.
Follow the Right Course
We must take it as a responsibility to follow the right course of getting things done rather than giving bribes to get them done speedily or to escape fines.
Install Cameras and Recorders
Technology can also help in bringing down corruption. CCTV cameras must be installed in government offices, at red lights, and other places where the cases of taking and giving bribes are high. Recorders can be installed at places where it is difficult to install cameras. People can also take the initiative to record any corrupt practice on their mobile and share it at their nearby police station.
Build Confidence
People in India are scared of going to the police, even for lodging a complaint against someone. They avoid going to the police station because they fear getting caught up in the nitty-gritty of the police inquiry, which may bring a bad name to them. The procedures at the police station must be such that those who wish to help the police must not face any inconvenience.
Conclusion
There are many ways to free India from corruption. Only the willingness to implement these ways is required.
Corruption Free India Essay 4 (500 words)
Introduction
The rate of corruption in India is quite high. Among other things, corruption impacts the growth and development of the country negatively. Most developing countries are facing this problem. The government and individuals in these countries don’t understand that corrupt practices may benefit them to some extent, but it hampers the growth of the country as a whole and is ultimately bad for them.
Causes of Corruption in India
There are several reasons why the corruption level is high in our country. Here is a brief look at these reasons:
Lack of Job Opportunities
The jobs in the market are less compared to the number of qualified youths. While many youths these days roam around without any jobs, others take up jobs that are not at par with their qualification. The dissatisfaction amongst these individuals and their quest for earning more leads them to take up corrupt means.
Lack of Strict Punishment
People in our country get away with corrupt practices such as giving and taking bribes, not paying the income tax, following corrupt means to run businesses, etc. There is no strict law to monitor the activities of people. Even if people get caught, they are not punished severely for it. This is the reason why corruption is high in the country.
Lack of Education
A society filled with educated people is likely to face less corruption. When people are not educated, they use unfair and corrupt means to earn their livelihood. The lower classes in our country undermine the importance of education, leading to increased corruption.