The Roll Logistics module of MPS Roll Handling is a complete roll logistic system that automates all movement of the rolls from their identification at the goods-in station to their use at the reelstands and on to the disposal of the core.
The Roll Logistics module is itself a collection of sub-modules that can be configured to cover whichever parts of the process the customer wishes to cover. These include: the main storage, the preparation station, the intermediate storage and the disposal.
The roll requirements of upcoming productions are obtained from the press management system MPS Production. The Roll Logistics module then ensures that the required rolls are automatically transported from the main storage to the preparation station, to the intermediate storage and on to the reelstands at the correct time.