IntraLog Summit 2024

Intralog Summit 2024

Event photos

An event organised by ABB, Ferag, Miebach, Vanderlande and Viastore to provide in-depth knowledge of the technologies that are revolutionising the intralogistics sector.

At this event, we presented success stories of intralogistics automation, new technologies and trends in the sector. There was also the opportunity to witness live demonstrations of mobile and industrial robotics.

In addition, we had the participation of companies such as Amazon, Auchan and Vegalsa-Eroski in a round table in which they shared their experiences with logistics automation.

The event took place on Wednesday 30 October 2024 at ABB's AMR Center in Madrid.

 

Highlights of the day

Agenda

9.30 - 10.00 h: Reception/Coffee

10.00 - 10.15 h: Welcome speech by Alfonso González, Managing director of AMR ABB

10.15 - 11.15 h: Session 1

  • Viastore: "Automated pallet storage as the buffer of the system"
  • Vanderlande: "Automated order picking in food retail"

11.15 - 11.45 h: Coffee Break

11.45 - 12.45 h: Session 2

  • Ferag: "Omni-channel order picking solutions"
  • ABB: "Added value of stationary and mobile robotics in intralogistics automation"

12.45 - 13.45 h: Round table: "Challenges in an intralogistics automation project"

Participants

  • Rolf Endres, Principal & partner at Miebach
  • Fernando Casal, Logistics director at Vegalsa - Eroski
  • Javier García Cerrada, Solutions designer manager at Ferag
  • Raimundo González, Director Supply Chain and Organization at Auchan
  • Vladimir Limo, Site Leader at Amazon

13.45 - 15.00 h: Lunch Break

15.00 - 16.00 h: Guided tour of the AMR showroom with demos

Do you want to learn more?