Commissioning
A robot that is well commissioned will run better, more reliably, use less energy and have a longer life.
Commissioning is not complicated for the experienced ABB specialists. They know how to get the most out of a robot, for example, reducing cycle-time, while keeping motor torques at an acceptable level.
Our specialists are on-hand at all phases of commissioning. They ensure that the robot is configured and efficiently integrated into the production system, and they provide full installation testing and assistance with the production start-up.