Global site

ABB's website uses cookies. By staying here you are agreeing to our use of cookies. Learn more

ABB’s MicroSCADA Pro

Benefit from the complete functionality, flexibility and support for monitoring and control of power systems of all sizes

MicroSCADA Pro automation solution provides complete functionality for monitoring and control of power systems of all sizes; such as Distribution Substation Gateways, Advanced Transmission Substation Automation systems and large Distribution Management Systems. The functional flexibility enables you to start with a basic set of features and later integrate additional functionalities according to your needs. The installed base of tens of thousands of licenses underline the proven experience and the unique opportunity for a strong local support network worldwide.

As a technological forerunner, MicroSCADA Pro has been one of the pioneers of the IEC 61850 deliveries and integration of different IEC 61850 devices as well as implementation of top class cyber security features to protect the automation systems.

The latest developments on MicroSCADA Pro increase the operational safety and utilize the benefits from the latest IEC 61850 enhancements

Enhanced authority allocation allows to manage operators’ control authority, leading to better operational safety of the grids. Operators’ control authority can be defined freely according to, for example, geographical locations, voltage levels or sub-systems, with secured access rights. The system can also ensure that there is only one operator with control authority at a time for a particular area and that no areas of the network are left without an operator. The control authority can also be exchanged between operators on the fly, either by themselves or by a master operator. As operators’ roles and responsibilities are clearly defined, the risk for operational mistakes is minimized and the quality of service and personnel safety is improved.

MicroSCADA Pro also continues to harvest the power of IEC 61850 by introducing enhanced support for IEC 61850 edition 2 features such as setting of substituted values, test mode and service tracking events from IEDs. The compliance to the standard is also reassured by the recent Edition 2 compliance certificate from DNV GL/KEMA.


Mikael Molander
Global Product Manager

E: mikael.molander@fi.abb.com

I am the Global Product Manager responsible for system products within Network Automation and Substation Automation domains today covered by the MicroSCADA Pro product family. I have more than 25 years of experience of automation of power systems after working across various R&D functions, global technology coordination and Product Management. My devotion is in understanding the users real needs and challenges and in developing solutions for these needs with superior user experience.
Call us!
Need more information? Call us today at +1-800-868-0497 or request a call back by filling the form below:

Comment on this article

Links and downloads