Global site

ABB's website uses cookies. By staying here you are agreeing to our use of cookies. Learn more

Applying differential protection to converter transformers

Spotting the difference no matter the (phase) angle

Standard Differential protection relays (IEDs) may have problem when applied on a Converter Transformer, which can have the phase shift different from standard 30 degrees (e.g. 7.5 degrees). Applying differential protection to such special transformer is difficult, but not impossible as demonstrated in a paper from Zoran Gajić of ABB Sweden.

Converter transformers, used to supply MV drives or feed into a power electronics devices (FACTS), don’t follow the usual transformer pattern of having a phase shift angle which is multiple of 30 degrees. The low voltage windings can be phase shifted for almost any angle, but most commonly used have (7.5 degrees).

That causes problems for standard transformer differential protection IED, which (in that example) will get a constantly-false differential current of 26 per cent of the through load current. To prevent false operation the differential protection pickup will have to be set to twice that, resulting in a system with very low sensitivity which is very important to be able to detect low level internal faults, such as winding turn to turn faults.

In the paper, presented at Cigre Colloquium in 2013, Gajić provides three practical example circuits how to make such installations, along with the captured readings from the differential protection IED. Interposing current transformers are used to compensate for the non-standard phase angle shift, allowing the protection system to operate with much greater sensitivity.

The examples show how this technique can be applied to converter transformers at 18, 24 & 36 pulse, and how a standard differential protection IED can protect such special transformers.

The technique; using interposing current transformers to align the individual winding phase currents, demonstrably lets standard differential protection IED to be applied to converter transformers, and the paper concludes citing practical experience that such systems are already proving reliable in the field.

Read more here:
Practical Experience with Differential Protection for Converter Transformers



Zoran Gajić


Zoran Gajić was born in Serbia, former Yugoslavia in 1965. He received his Diploma Engineer Degree with honors in electrical power engineering from University of Belgrade, Serbia in 1990 and PhD degree in electrical power engineering from Lund University, Sweden in 2008. Read more about Zoran Gajić

Since 1993 he has been working in the area of power system protection and control within ABB Group of companies, where he had various engineering positions. Currently he has position of Global Product Manager for Transformer and Generator Protection with ABB SA Products in Sweden.

Dr. Gajić is a member of various Cigré Study Committee B5 and IEC/MT4 working groups. He has published numerous technical papers in the relay protection area. His main working areas are practical applications of protection relays, computer applications for protection and control of electrical power system, development of advanced protection algorithms for numerical relays and power system simulations. Zoran is holder/co-holder of several patents.

Call us!
Need more information? Call us today at +1-800-868-0497 or request a call back by filling the form below:

Comment on this article