Global site

ABB's website uses cookies. By staying here you are agreeing to our use of cookies. Learn more

Indirect measurement reveals rotor current

Measuring rotor DC without a resistive shunt

Generator_hall_800x270

Measuring current and voltage from a DC rotor has long been a challenge, generally requiring the use of a resistive shunt or other additional equipment. AC stator quantities, on the other hand, can easily be quantified with through Instrument Transformers.


In this work engineers from ABB and PD Drinsko-Limske HE used the output from a standard CT connected to the excitation transformer, which feeds the static exciter. That provides a measure of AC current, and from that information the team was able to program an ABB IDE to calculate the DC current of the rotor.

That information provides a hitherto unseen insight into the performance of the generator, enabling better understanding of its operation, but also to monitor for thermal overload, over-current protection, and under-current protection, of the rotor winding.

That was the theory, but to test it a measurement system was installed on one of a pair of 315MVA, 11kV, 426.6rpm, generator-motor units. Connections were made to both the LV and HV CTs, to maximize the data coming into the IED, which then used both measurements to calculate the DC current at the rotor twice, enabling the two sources of data to be compared.

A resistive shunt was also available, to check on the accuracy of the new system.

Not only did the new system match the DC voltage recorded by the shunt, but it also proved that CTs connected to the LV and HV sources produced the same calculated DC voltage. That is going to make for much cheaper and more accurate monitoring of rotor DC systems, and logging of detailed performance data for future analysis which should lead to improve generator operation.




Zoran Gajić


Zoran Gajić was born in Serbia, former Yugoslavia in 1965. He received his Diploma Engineer Degree with honors in electrical power engineering from University of Belgrade, Serbia in 1990 and PhD degree in electrical power engineering from Lund University, Sweden in 2008. Read more about Zoran Gajić

Since 1993 he has been working in the area of power system protection and control within ABB Group of companies, where he had various engineering positions. Currently he has position of Global Product Manager for Transformer and Generator Protection with ABB SA Products in Sweden.

Dr. Gajić is a member of various Cigré Study Committee B5 and IEC/MT4 working groups. He has published numerous technical papers in the relay protection area. His main working areas are practical applications of protection relays, computer applications for protection and control of electrical power system, development of advanced protection algorithms for numerical relays and power system simulations. Zoran is holder/co-holder of several patents.

For the latest news, articles and whitepapers on Substation Automation, simply enter your name and email address below:

Comment on this article

Links and downloads