Global site

ABB's website uses cookies. By staying here you are agreeing to our use of cookies. Learn more

Translate accurate data into always correct actions

Operating Time - Introducing opportunities of MicroSCADA Pro Historian functionality

Did you know that MicroSCADA Pro Historian supports calculation of operating time, also known as run time, on/off time of a device or the time an analogue measurement exceeds the set limits? All the above is based on the process information collected by the SCADA server and stored in the Historian.

You can set the operating time to be automatically aggregated to predefined and freely selectable time periods such as a minute, an hour, a day, a week, a month or a year. In data retrieval any time period is supported – for example, if you would like to find out when the temperature has been above 32 degrees during the last four days.

MicroSCADA Pro Historian

The operating time can be calculated from a primary device such as transformer, generator or rotating motor with any kind of pump, like a water leakage pump or an air pressure pump.  

To get a grip on the benefits of using operating time, let’s take a little bit closer look at the examples of some applications with pumps and transformers.

  • Pumps
    • Quite often we have an underground storage tank for water leaks, equipped with a leakage pump.  In normal conditions the leakage pump runs known, more or less equal time within a time period.  When analyzing the operating time with Historian we can identify the trend of leakage over a longer period and thus take preventive actions to avoid the problems of increasing leakage. The total run time can also be used to plan and define motor and pump maintenance schedules and actions. Let’s take yet another example. Air pressure is used in several applications and typically generated by an automated compressor and an air tank combination maintaining desired pressure level for operations.  In some applications incipient air leakage could be detected at an early phase by supervising the operating time trend.
  • Transformers
    • It is usually a preference for substations to be aware of how long each of their transformers has been energized and how the total energy flow has been shared between the available resources. In addition, the time the load has been above a user-defined limit - for example, over 115% of the nominal power and thus causing a severe overloading effect for a transformer - will provide valuable information about an aging transformer to the asset responsible.

Furthermore, in some cases it is of interest to have the knowledge about the maintained window of irrelevant voltage level or to present a voltage level duration curve.

As a summary, operating time can eliminate undesirable effects and help to follow the real-time condition of objects, to name but a few. Try out MicroSCADA Pro Historian yourself and let us know how operating time has benefitted you.



Editorial contact: Heidi Hautala









Mikael Molander

Mikael Molander
Global Product Manager


I am the Global Product Manager responsible for system products within Network Automation and Substation Automation domains today covered by the MicroSCADA Pro product family.

I have more than 25 years of experience of automation of power systems after working across various R&D functions, global technology coordination and Product Management. My devotion is in understanding the users real needs and challenges and in developing solutions for these needs with superior user experience.

Call us!
Need more information? Call us today at +1-800-868-0497 or request a call back by filling the form below:

Comment on this article

Links and downloads

  • Contact us

    Submit your inquiry and we will contact you

    Contact us