We report on the development of a modern numerical SSR protection to replace an existing
analogue relay that no longer could be adapted to changing operating conditions. The
development is based on knowledge gained from field recordings of SSR events at the
prospective site. From this and some theoretical considerations, it was possible to design a
new protection function that is more reliable than previous generations of SSR relays.
Sub- and super-synchronous current and voltage, torsional vibration, field measurements,
SSR protection.
Sub-synchronous resonance (SSR) can cause a growing pulsating torque on the generator
and turbines shaft. SSR can appear in thermal power units which have a long shaft and where
the generator is connected to a long radial transmission network with series capacitors. It is
considered as an unstable and dangerous condition that can cause fatigue and damage to the
shaft, in the worst case the shaft could even break. SSR in hydro power units are very unlikely
because the inertia of the generator is very dominant and the inertia of the turbine is only 5 to
10 % of the total inertia of the hydro power unit [1].
The initial interest in sub-synchronous resonance, caused by the first two famous catastrophic
events in 1970 and 1971 [2], has in the past decades diminished considerably. Nevertheless
there are still major generating plants located in vicinity of series compensated transmission
lines and/or HVDC converter stations which may be vulnerable to this phenomenon.
Even in cases where protection already exists, any changes in the power system may raise
SSR-specific concerns again. Such changes include changes or replacement of the generator
or any turbine section (HP-, IP- or LP-section). The changes may also include changes of the
network structure or degree of compensation of adjacent series compensation transmission
lines or an unusual switching state in the transmission network. In such a case, an existing
SSR protection system may need re-tuning which may be a delicate process.
In this paper, we report on such a case, where the detailed know-how on the tuning procedures
for the existing protection were no longer available, as it was designed and installed around
2
1985. Furthermore, suitable replacements could not easily be found on the market. Therefore
an entirely new SSR protection had to be developed.
In the following, the development process is discussed in some detail. First we give an
overview of the prospective site and then describe observations from captured SSR events
which led to some theoretical derivations. The total information gathered enabled a rather
unconventional design of the final protection function.
In the Swedish national grid there are ten series compensated lines. Eight of them are
transmission lines connecting the north to the southern part of Sweden. The other two lines
are connections between Sweden and Finland. Studies have shown that three of these ten
series compensated lines can cause sub-synchronous resonance (torsional interaction)
between a generator unit in Forsmark Nuclear Power Plant (NPP) and the electrical grid, see
Figure 1.
The length of these three series compensated
lines is around 300 km and the compensation
degree is between 70-85 %. They are
connected to Ängsberg and Stackbo 400 kV
substations, which are located at a distance of
around 70 km from the Forsmark NPP. A 400 kV
converter station for HVDC link to Finland is
also located in the vicinity of Forsmark NPP.
At the Forsmark NPP-site there are three boiling
water reactors designed by Asea-Atom.
Forsmark 1 entered into commercial operation
in 1980, while Forsmark 2 began operating
commercially in 1981. Forsmark 3 began
commercial operation in August 1985. The only
unit that is sensitive to the sub-synchronous
resonance is the 3rd unit which is the largest,
rated around 1240 MWe and producing 9 TWh
annually. During last years a modernization
project has been ongoing. Due to foreseen shaft
changes the original shaft mechanical torsional
frequency will change and corresponding
changes in the presently used SSR relays are
unavoidable.
The existing SSR protections were installed in
the middle of the 1980:s. They are installed at
the three series capacitor stations and at the
NPP [3]. Relays at 400 kV monitor currents in two phases and have a filter with pass-band of
17–36 Hz. The filter is connected to an over-current function with inverse time characteristic.
This old protection has limited setting ranges and the filter characteristic is not adjustable.
Currently the following approach for long lasting SSR events is used in Swedish power system:
First the SSR relay in the 400 kV station shall operate in order to bypass the series capacitors.
However, if this action do not stop the SSR oscillation, the relay at the NPP shall give a trip
command to the affected generator in order to save the unit shaft from fatigue.
Steelworks with arc furnaces are also situated close to Ängsberg and Stackbo substations.
These arc furnaces cause a lot of noise in measured voltage and current signals below 50 Hz
which can cause unwanted operation of the SSR relays. The Swedish railway system operates
at 16.7 Hz which also has to be taken into account when designing new numerical SSR
protection relay.
The design of any protection function requires deep insight into the addressed phenomenon
which can be obtained from literature, simulations and site measurements. When the project
to develop a new SSR protection relay was formed, it was possible to mainly rely on the last
approach. Thus two modern protection Intelligent Electronic Devices, IEDs, where installed,
one at the generating plant and one at the 400 kV substation. Initially, these two IEDs where
only functioning as disturbance recorders trigged by the start signal from the existing SSR
relays. When the new software functionality, discussed in Section 5, became available, this
was also used to trig disturbance records. This enabled a first comparison between the
performance of the existing and the conceived numerical SSR protection. The numerical
design of the new relay also allowed logging of SSR quantities over longer period of time
(months) on a stand-alone PC. In a final stage of the project a new numerical SSR protection
functionality with all desired logics was installed.
This section intends to give some brief highlights of the observations made from disturbance
records and logs. Examples will be provided that shows active SSR phenomena, how they
may be initiated and how long they can persist. A comparison of the existing and new SSR
relay will be presented. Also an example of a non-SSR disturbance that may cause an
unwanted operation of the SSR relay is given.
Many of the observed SSR events are initiated by relatively fast load changes or network
transients. Such transients have namely a very wide frequency content and if they are strong
enough, they may initiate mechanical torsional oscillations of the unit shaft. These events are
good examples of how an SSR event can be identified, as initially there are no SSR current
and voltage components present while they are observed after the transient. An example with
a known cause is chosen here; it is caused by a quick and large ramp-down of the nearby
HVDC link due to a system contingency in Finland.
In Figure 2 the voltage and current frequency spectrum, as recorded at the generator terminals,
before and after the switching transient are presented. Amplitudes are given in percent of CT
and VT rating. The peaks appearing around 17, 83 and 117 Hz are caused by the Swedish
railway system, operating at 16.7 Hz. Note that several new peaks, caused by SSR, have
appeared around the fundamental frequency after the switching transient.

The figure shows that initially the frequency region between 20 and 40 Hz is without any
detectable peak magnitude. However, after the transient, the spectra to the right in Figure 2 is
obtained. Here, several peaks symmetrically distributed above and below the fundamental
frequency have appeared. The symmetrical distribution is a natural consequence of the
modulation caused by torsional vibrations in the generator shaft, as will be shown in Section 4
below. This is thus a good indicator of an on-going SSR phenomenon while the symmetric
peaks have not attracted much attention in the existing literature [2,3,4]. Several peaks appear because a unit shaft with multiple turbines will have a number of torsional resonance modes,
see references [2,4] for a detailed discussion.
The torsional oscillation modes have different damping characteristics so that only the
strongest can be observed in a disturbance record trigged half a minute later. This mode,
mode-3 in Figure 2, has the largest potential to cause dangerous SSR events and will be the
main focus of the further discussion in the paper. The other two modes, especially mode-2,
should not be totally neglected, however.
Most of the SSR events initiated by transients decay rather quickly, the present example is
rather unusual in that it persist for more than 30 seconds as proven by the subsequent
disturbance record. Figure 3 show the initial decay of the torsional mode-3 as seen by suband
super-synchronous currents and voltages. From these figures, it is notable that the suband
super-synchronous current components have almost identical amplitude, whereas the
super-synchronous voltage component has about twice the amplitude of the sub-synchronous
voltage component. This observation will be further exploited in Section 4.

The disturbance records were generally trigged by a high current in the frequency range below
the fundamental. There are however other phenomena that may cause high sub-fundamental
currents as shown in Figure 4. The broadness of the current peak below fundamental
frequency and the lack of a mirror peak above, clearly indicate that this is not caused by SSR.
A possible cause may be a steelwork using an electric furnace in the vicinity of the substation.
Disturbances such as this may cause an unwanted operation of the SSR protection and must
thus be considered in the new relay design.
A transient-induced SSR event was discussed in some detail above, such events generally do
not cause very large SSR currents and usually decay within a few seconds, inducing limited
strain on the unit shaft. Indeed, the transient itself is often a much larger ordeal. However,
disturbance records with almost constant SSR activity are also recorded. Many of these are
from relatively short time periods, while there are much longer spans between these bursts of
SSR recordings. This is understood as a persistent SSR event and durations up to 10 hours
are indicated by some disturbance record sequences. As disturbance records only give a few
seconds snapshot when the SSR level has passed a trigger criterion, they are not well suited
for studying persistent SSR. Most importantly, persistent SSR with amplitude that is always
above any trigger criterion may only give a disturbance record at start and thus pass largely
unnoticed.
It is thus interesting to log the sub-synchronous amplitudes continuously and with the new
numerical IED design, this became possible. A computer connected to the same
communication network as the IED can then read the sub- and super-synchronous voltage,
current and frequency from the new functionality and write them to a time-stamped log file.
Such logging systems where installed both at the Forsmark NPP and the 400 kV substation.
One prolonged SSR event that is logged in both places will be discussed below.
As seen from Figure 5, the selected SSR event lasted more than 30 minutes. In contrast to the
previous example, there is no clear indication of an initiating transient or any hint of why it
ended from the captured disturbance records. The observations from the two sites are
remarkably similar while the SSR amplitudes are relatively smaller at the 400kV substation.
In view of the sub- and super-synchronous amplitude relations at the generator terminals for
the transient event shown above, it is interesting to compare spectra from the 400kV substation
and from the generator terminals, such are shown in Figure 6. Here it is obvious that the suband
super-synchronous components propagate quite differently in the power grid and the SSR
voltage peaks may not be so clearly visible at the 400kV substation.
When an existing protection function is to be replaced, it is of course important to verify that
the new function has at least the same capabilities as the old SSR relay. This may become a
very complex task if all aspects of the functionality, such as bandwidths, time delays, etc., are
to be compared. Thus, only the sensitivity to SSR currents is evaluated in the paper.
The evaluation is based on disturbance records captured by the IED with the new software
functionality running. The estimated amplitudes for SSR currents and voltages are saved in the record together with digital channels reflecting trigger criteria from over-voltage or overcurrent
based on the estimated amplitudes. From the existing SSR protection, only the start
signal via a contact was available, thus the only information is that the existing analogue SSR
over-current relay has seen a larger SSR signal than its set start threshold. Start levels for the
new design and the existing SSR relay were set to the same current level, about 0.12% at the
generating plant, whereas the trip level is about 0.45%. The start level of the existing protection
at the 400 kV substation is somewhat higher. Start signals from both the existing protection
and the new SSR functionality could trig disturbance records.

From the analysis of a large number of disturbance records from the generating plant it is found
that both functions issue start signals if the current is large enough, larger than 0.4%. A case
was found where the existing protection issued a start signals for an SSR current as low as
0.05% as estimated by the new SSR relay whereas it did not react to a case with 0.38%
estimated current. No case was found where the existing protection had issued a start signal
and the new SSR relay could not find a significant SSR current. It is no surprise that the two
functions estimate the SSR current somewhat differently as they are based on very different
principles: the existing protection use analog filters whereas the new SSR relay is a numerical
algorithm with no direct analog correspondence.
Thus it is assured that the new numerical SSR protection is designed to react for SSR currents
with the same sensitivity as the existing protection. Appropriate time delay in the form of
inverse time characteristics can easily be provided with numerical design. Furthermore, the
findings from this investigation present possibilities to design a more reliable SSR protection.
To summarize the observations made:
-
Sub-synchronous resonances have been observed both at the generator terminals and
at 400kV transmission substation.
- The existing and new numerical protection reacts reasonably consistent to SSR currents.
- Both sub-synchronous and super-synchronous peaks are observed for SSR currents
and voltages. The relation between these peaks seems to have a simple relationship at
the generator terminals, whereas at the 400kV substation a predictable pattern is not as
obvious.
- SSR events are often initiated by sudden load changes but these events usually decay
rapidly; in some cases more persistent resonances are initiated. An SSR protection
function should thus not react too rapidly as the presence of a resonance cannot be
established while a system transient occurs.
- SSR activity may last for a long time, several hours. It may appear and disappear without
any obvious external reason.
- SSR protection purely based on sub-synchronous current level may be affected by other
system disturbances and noise.
The apparent relation between the sub- and super-synchronous amplitudes observed in Figure
3 demands a theoretical study. Consider thus a simple model of a single-phase synchronous
machine and assume that the field-winding generates an air-gap magnetic field with the peak
value Bm
and that the air-gap flux varies sinusoidally in tangential direction around the
periphery of the rotor body. Assume also that the mechanical angular velocity of the rotor varies
sinusoidally around the average angular velocity ωn
with the angular velocity ω p
(a torsional
mechanical resonance). The instantaneous angular velocity is then given by:
where ∆Ω is the peak value of the deviation of the instantaneous mechanical angular velocity from the average angular velocity ωn . After integration of the argument of the sinusoidal function and application of Faraday's law of induction, the induced voltage (tu ) in the stator is given by:
where A is a constant depending on the area of the stator winding and the number of turns. Expanding the derivatives and performing a series expansion gives an expression for the stator voltage to first order in ∆Ω:
From this expression we note that there is a relation between the sub- and super-synchronous voltage component amplitudes and their respective frequencies as per the following equation:
The voltage components amplitude ratio is hence equal to the ratio of the frequencies, which
is roughly what is observed for the SSR voltages in Figure 3. Such a relation is thus a simple
evidence that SSR is observed which can be exploited to design a more reliable SSR
protection. Furthermore, the ratio of SSR amplitude to the fundamental frequency voltage is
only dependent on the involved frequencies and the vibration amplitude∆Ω. The voltage SSR
amplitudes can thus be used as a direct measurement of the torsional vibration amplitude.
If the generator load at off-nominal frequencies is dominantly inductive, the absolute load
impedance will linearly increase with frequency. Thus the currents at sub- and supersynchronous
frequencies will be approximately equal, again as observed in Figure 3.
It must be strongly emphasized that this derivation only holds for sub- and super-synchronous
voltage and current components at the generator terminals. In the transmission grid, these
relations become much more complicated and depends on the particular network details.
The biggest challenge for any type of SSR relay is its capability to accurately measure the SSR
current and/or voltage components. As shown in this paper these components can be
extremely small (less than one percent of the CT and VT rating). However it shall be noted that
8
the fundamental frequency current and voltage, which are always present during an SSR
event, serve as a carrier signal for the SSR components throughout the whole measurement
chain including input CTs and/or VTs of the numerical IED. Thus their presence effectively
enables the SSR relay to measure at all such small current and voltage quantities. At the same
time the measurement/filtering part of the SSR relay itself must be capable to suppress the
fundamental frequency component in order to extract the SSR component with high precision.
Therefore a special digital filter was implemented in the new SSR relay. By using long
measurement windows (about one second) and special window filtering technique it was
possible to design a digital filter which is capable of extracting the sub- or super-synchronous
voltage or current components [5]. The new filter delivers the phasors (magnitude and the
phase angle) and the frequency of the extracted components for all three phases from the
connected CT and/or VT circuits. Then, in order to realize a SSR protection, these SSR
component phasors are given to the standard over-current or over-voltage functions which
provide the required timing for the SSR relay operation. Note that over-current and/or overvoltage
functions are readily available in the modern numerical IEDs. Typically a special
Inverse Definite Minimum Time (IDMT) curve is used for SSR protection [3]. The required
inverse timing operating characteristic is easily provided by the programmable IDMT curve of
the standard over-current or over-voltage protection functions. The frequency of the SSR
component which need to be extracted by the filter is only a setting parameter. Thus the new
numerical relay [5] can easily be adapted to any SSR installation.
The observation found from the field studies is that the SSR voltage magnitude at the generator
terminal is directly proportional to the shaft torsional vibration amplitude, while the SSR current
magnitude is dependent on the impedance of the connected power system. Therefore it was
decided to use the SSR voltage components within the new SSR protection relay for tripping
logic. As stated previously the standard over-voltage functions are used to provide necessary
IDMT time delay. The following figure provides simplified logic diagram used within the new
SSR relay installed at the generator terminals on Unit 3 in Forsmark NPP. The logic shown in
Figure 7 can be summarized in words as follows. The first two filters are used in order to extract
mode-2 super- and sub-synchronous SSR voltage components. The mode-2 supersynchronous
voltage component (USUP_2) is then given to the standard over-voltage function in order to provide the IDMT time delay. Once this IDMT time delay has expired and at the same
time the mode-2 sub-synchronous voltage component (USUB_2) is bigger than the set threshold
the Trip command will be given from the new SSR relay.

Filter number three and four are used to provide the same functionality for mode-3 super- and
sub-synchronous SSR voltage components. Finally the fifth and sixth filter are used to extract
super- and sub-synchronous SSR current components. These current components are not
used for tripping logic but only for alarm purposes.
However, it should be noted that the logic presented in Figure 7 will only be used for the new
SSR relay installed at the generator terminals. For reasons explained previously in this paper,
the new SSR relay installed in the 400kV substation will still use only the sub-synchronous
current components for its operation.

This project has proven that it is possible to design a numerical SSR protection relay on a
standard hardware platform. The new SSR relay has
shown performance practically identical or even
better than the old analogue SSR relay. Due to
modular numerical design the new SSR relay can be
easily adapted in different installations. The numerical
SSR relay [5], utilizing the logic presented in Figure 7,
is installed on Unit 3 in the Forsmark NPP. The
protection panel used in this installation is shown in
Figure 8.
In addition to the new SSR relay (indicated by number
one in Figure 8), a separate logging system is also
installed (indicated by number two in Figure 8). This
logging system writes continuously (once every two
seconds) the SSR sub- and super-synchronous
current and voltage components as well as their
frequencies to the industrial PC hard disk.
Additionally, the system provides trending features
which can be displayed directly on the screen
available in the panel (indicated by number three in
Figure 8). This will enable the Forsmark NPP
personnel to get a quick overview of the SSR
activities in the Swedish power network in the future.
- G. Andersson; R. Atmuri; R. Rosenqvist; S. Torseng, “Influence of Hydro Units' Generator-toTurbine Inertia Ratio on Damping of Subsynchronous Oscillations”, (IEEE Transactions on Power Apparatus and Systems, vol. PAS-103, no. 8, pp. 2352-2361, August 1984)
- P.M. Anderson, B. L. Agrawal, J. E. Van Ness, “Subsynchronous resonance in power systems”, (IEEE Press, ISBN 0-7803-5350-1)
- Westinghouse Electric Corporation, “SSO Relay”, (Application Data 40-174, December 1984)
- P. Kundur, “Power system stability and control”, (McGraw-Hill 1994, ISBN 0-07-035958, Chapter 15)
- ABB, “Technical Manual for Generator protection REG670 2.0 IEC”, (Document ID: 1MRK 502 052-UEN; May 2014)