Global site

ABB's website uses cookies. By staying here you are agreeing to our use of cookies. Learn more

Upgrading reliable sensor technology with a modern IEC 61850 process bus

Digital substations upgrading

REFERENCE CASE STUDY

The Australian electricity transmission company Powerlink Queensland owns and operates Queensland’s high voltage electricity transmission network. In this digital substation project, ABB drew on its extensive experience with non-conventional instrument transformers (NCITs) to replace the originally installed proprietary process bus with IEC 61850 technology and connected the primary (high-voltage) equipment to the substation protection and control devices more effectively, improvig the reliability and availability of the optimized substations.

In 2011 the first commercial process bus installation, the so called digital substation, was successfully put into operation. This first digital substation outside of China was only the first of a series of six outdoor substations with process bus and NCIT technolgy. The second and the third substations were put in service in 2013 and 2014 respectively.

In this project, Powerlink Queensland makes use of the SAS600 station automation system from ABB, Relion® 670 series protection and control IEDs and the REB500 distributed busbar and breaker failure protection system.

All protection and control equipment in the system are connected to the IEC 61850-9-2 process bus and receive analog sampled values from the CP-MU merging units also supplied by ABB. New sensor electronics connect the MUs to the existing combined current and voltage sensors. This approach allowed the refurbishment of the primary technology to be kept to a minimum.

Thanks to the integrated redundancy of the NCITs from ABB, two completely independent systems of merging units and protection equipment were implemented to meet the customer’s redundancy requirements.

The replacement of copper wires by fiber optic cables and the description of the transferred information according to IEC 61850 opened new opportunities for intelligent testing tools to support the commissioning and maintenance of the substation. 

Installed protection and control equipment


Additional experience in digital substation


In addition to the described projects, ABB installed several pilot installations to prove further products from ABB‘s digital substation offering, like FOCS, the optical current transformer and to help customers gain experience with this technlogy.

The modernization of the installations with the latest technology in accordance to IEC 61850 supports Powerlink Queensland in its mission to responsibly deliver electricity transmission services that are valued by shareholders, consumers, customers and the market.
Device Function
Process level
ELK-CP Non-conventional redundant instrument transformers for current and voltage measurement in gas-isolated switchgear
CP-MU Non-conventional redundant instrument transformers for current and voltage measurement in gas-isolated switchgear
Bay level
REC670 Bay control IED
REL670 Line distance protection IED
RED670 Line differential protection IED
RET670 Transformer differential protection IED
REB500 Busbar and breaker failure protection system
Station level
RTU560 Communication gateway to control center
MicroSCADA Pro Substation automation system
Auxiliary facilities
Building Transportable building for protection and control cabinets, automation system and auxiliary facilities

Safety


  • The modernization of the installations with the latest technology in accordance to IEC 61850 supports Powerlink Queensland in its mission to responsibly deliver electricity transmission services that are valued by shareholders, consumers, customers and the market.

Compliance


  • These deliveries bring Loganlea Substation into full compliance with the most advanced global standard for substation automation, maximizing availability and grid reliability.

Future-proof investment


  • With demand for electricity growing fast, Queensland needed to further build on long-term, cost effective solutions for its power system. By upgrading the substation with advanced automation and the latest communications standards, ABB helped Powerlink to fulfill its strategy well into the future.

Related links

  • Contact us

    Submit your inquiry and we will contact you

    Contact us