ABB launches VD4-AF, a new vacuum circuit breaker for steel furnaces

ABB launches VD4-AF, a new vacuum circuit breaker for steel furnaces

High-performance features enable relentless operation and protection for steel furnaces at lower costs.

ABB enhances its portfolio of medium-voltage circuit breakers with VD4- Arc Furnace, a unique solution based on vacuum technology and innovative actuation systems, to provide a new high quality, reliable and efficient solution.

The VD4-AF circuit breaker, which performs up to 150,000 close-open operations, ensures zero downtime for breaker overhaul thereby reducing total costs of the furnace operation. The embedded control unit enables optimized operations with servomotors, increasing the circuit breaker’s performance by up to ten times of what could be previously achieved.

“We recognize the steel manufacturer’s daily challenges to boost output and increase utilization levels of assets,” said Matteo Caiti, Global Product Group Manager, Control and Protection Products for ABB. “The VD4-AF solution enables their operations to run continuously to produce the highest quality product.”

The VD4-AF circuit breaker is designed with a draw-out, roll-on-floor construction, to be combined with the ABB PowerBloc enclosure. This allows a faster and easier integration or replacement operation. This together with the 150,000 close-open operations result in more than a 50 percent reduction to the frequency and duration for inspection or maintenance, compared to any other solution.

Additional features include:

  • Embedded advanced diagnostics
  • Up to 38 kV, 2500A, 31.5 kA
  • Built-in interlocks

Detailed information about VD4-AF circuit breaker, its advantages and main features is also available at the product webpage.

ABB (ABBN: SIX Swiss Ex) is a pioneering technology leader in electrification products, robotics and motion, industrial automation and power grids, serving customers in utilities, industry and transport & infrastructure globally. Continuing a history of innovation spanning more than 130 years, ABB today is writing the future of industrial digitalization with two clear value propositions: bringing electricity from any power plant to any plug and automating industries from natural resources to finished products. As title partner of Formula E, the fully electric international FIA motor-sport class, ABB is pushing the boundaries of e-mobility to contribute to a sustainable future. ABB operates in more than 100 countries with about 135,000 employees. www.abb.com

Links

Contact us

Downloads

Share this article

Facebook LinkedIn X WhatsApp