Identification of On-Site Parameter Changes
ABB Field Information Manager Learning Center
Field Information Manager supports an automatic On-Site Parameter Scan in the background to check devices for parameter changes made on-site in devices, e.g. with a handheld or local device panel.
The On-Site Parameter Scan is enabled by default and can be configured via Tools Menu - PROJECTS - PROCESS COCKPIT.
The scan iterates over all connected field devices in an interval of 30 seconds, i.e. it takes 300 seconds (= 5 minutes) to iterate over a complete example topology with 10 field devices.
The On-Site Parameter Scan can also be started manually for one or multiple devices via Device Tile Context Menu - MORE - ON-SITE PARAMETER SCAN, e.g. to prioritize the selected devices.