Use this option if you want to import or export an Offline Dataset or Template. The export file will contain the dataset and the used Device Package as well. This ensures that the import on a different computer node will succeed even if the Device Package is not available on that node.
Importing a dataset from a file:
For importing a dataset from a file, please drag & drop the *.fim file into the Field Information Manager main frame, which will start the import automatically.
Export a dataset into a file:
- Access the dataset and open the Context Menu.
- Select OFFLINE and EXPORT.
- Specify the file location and the file name and confirm.