Device Views are available for physically connected devices or for offline Device Datasets.
The Device View header contains the word –DEVICE– if the view connects to a physical device, or the view header contains the work –OFFLINE– if the view connects to an Offline Dataset.
Most of the device views provide status information in front of the input element. The tooltip of these elements provides more details about the status. The following status information is available: