Standard Symphony Plus Workstations

Windows Server 2016 and Windows 10 LTSC 2016

In this section, it’s possible to find all the workstations that can support the following Operating System: Windows 10 LTSB 2016.

The machines are grouped in two tabs accordingly to their physical features and configurations:

  • PREMIUM AND PRECISION
  • EFFICIENT

Finally, for each tab there are machines chosen between two different suppliers.

PREMIUM AND PRECISION
EFFICIENT

These models are suitable for:

  • Extra Small Systems (i.e. max 5000 tags)
  • Applicable for S+ Standalone installation, S+ Engineering or S+ Operations Server and S+ Engineering or S+ Operations client profiles.
  • Optional add-on kit for rack mounting: with rack kit it is possible to mount the machine on a cabinet

This model is useful when the load for the client machine is not heavy.

Premium and Precision models are more performant but also more expensive, so Efficient machine is a good tradeoff considering the right balance between limited budget and not excessive stressing of the node.

 

Select region / language