Machining Software is an easy-to-use tool that allows engineers to manage and monitor robots used in machining tasks such as laser, water jet, and mechanical cutting, as well as deburring. The Machining Standard version offers three types of auto-calibration for toolkits, cutter, cross beam and work objects. The Premium package also offers path-tuning, enabling users to easily fine-tune paths and edit thousands of path points, shortening the process from more than two days to just half a day.
The exclusive ABB polyhedron-based calibration allows for enhanced accuracy in the rotational aspect, making it an ideal work object calibration method for applications in machining, polishing, and dispensing.